LFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
       Definition at line
       
        2367
       
       of file
       
        em_cmu.h
       
       .
      
      
       #include <
       
     
        em_cmu.h
       
       >
      
         Data Fields | 
       |
| uint8_t | ctune | 
| uint8_t | gain | 
| CMU_OscMode_TypeDef | mode | 
| uint8_t | timeout | 
Field Documentation
| uint8_t CMU_LFXOInit_TypeDef::ctune | 
CTUNE (load capacitance) value
        Definition at line
        
         2369
        
        of file
        
         em_cmu.h
        
        .
       
Referenced by BSP_initClocks() , and CMU_LFXOInit() .
| uint8_t CMU_LFXOInit_TypeDef::gain | 
| CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode | 
| uint8_t CMU_LFXOInit_TypeDef::timeout | 
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_cmu.h