QSPI Device Write Instruction Configuration Structure.
       Definition at line
       
        110
       
       of file
       
        em_qspi.h
       
       .
      
      
       #include <
       
     
        em_qspi.h
       
       >
      
         Data Fields | 
       |
| QSPI_TransferType_TypeDef | addrTransfer | 
| bool | autoWEL | 
| 
         Enable/disable automatic issuing of WEL (Write Enable Latch) command before a write operation.
          | 
       |
| QSPI_TransferType_TypeDef | dataTransfer | 
| uint8_t | dummyCycles | 
| uint8_t | opCode | 
Field Documentation
| QSPI_TransferType_TypeDef QSPI_WriteConfig_TypeDef::addrTransfer | 
Transfer type used for address.
        Definition at line
        
         118
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_WriteConfig() .
| bool QSPI_WriteConfig_TypeDef::autoWEL | 
Enable/disable automatic issuing of WEL (Write Enable Latch) command before a write operation.
When writing to a flash device, the WEL within the flash device must be high before a write sequence can be issued. The QSPI peripheral can automatically issue the WEL command before triggering a write sequence. The command used for enabling the WEL is WREN (0x06) and is common between devices.
        Definition at line
        
         134
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_WriteConfig() .
| QSPI_TransferType_TypeDef QSPI_WriteConfig_TypeDef::dataTransfer | 
Transfer type used for data.
        Definition at line
        
         121
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_WriteConfig() .
| uint8_t QSPI_WriteConfig_TypeDef::dummyCycles | 
Number of dummy read clock cycles.
        Definition at line
        
         115
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_WriteConfig() .
| uint8_t QSPI_WriteConfig_TypeDef::opCode | 
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_qspi.h