LCD Animation Configuration.
       Definition at line
       
        241
       
       of file
       
        em_lcd.h
       
       .
      
      
       #include <
       
     
        em_lcd.h
       
       >
      
         Data Fields | 
       |
| LCD_AnimLogic_TypeDef | animLogic | 
| uint32_t | AReg | 
| LCD_AnimShift_TypeDef | AShift | 
| uint32_t | BReg | 
| LCD_AnimShift_TypeDef | BShift | 
| bool | enable | 
| int | startSeg | 
Field Documentation
| LCD_AnimLogic_TypeDef LCD_AnimInit_TypeDef::animLogic | 
A and B Logical Operation to use for mixing and outputting resulting segments.
        Definition at line
        
         253
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_AnimInit() .
| uint32_t LCD_AnimInit_TypeDef::AReg | 
Initial Animation Register A Value.
        Definition at line
        
         245
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_AnimInit() .
| LCD_AnimShift_TypeDef LCD_AnimInit_TypeDef::AShift | 
Shift operation of Animation Register A.
        Definition at line
        
         247
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_AnimInit() .
| uint32_t LCD_AnimInit_TypeDef::BReg | 
Initial Animation Register B Value.
        Definition at line
        
         249
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_AnimInit() .
| LCD_AnimShift_TypeDef LCD_AnimInit_TypeDef::BShift | 
Shift operation of Animation Register B.
        Definition at line
        
         251
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_AnimInit() .
| bool LCD_AnimInit_TypeDef::enable | 
Enable Animation at end of initialization.
        Definition at line
        
         243
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_AnimInit() .
| int LCD_AnimInit_TypeDef::startSeg | 
Number of first segment to animate. Options are 0 or 8 for Giant/Leopard. End is startSeg+7.
        Definition at line
        
         256
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_AnimInit() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_lcd.h