EZRADIODRV_FieldLength Struct Reference
EzRadio transmit field length sturcture. Holds length information on all available fields. Data is got from the generated radio configuration header file.
       Definition at line
       
        82
       
       of file
       
        ezradio_transmit_plugin.h
       
       .
      
      
       #include <
       
     
        ezradio_transmit_plugin.h
       
       >
      
         Data Fields | 
       |
| uint8_t | f1 | 
| 
         Field 1 length.
          | 
       |
| uint8_t | f2 | 
| 
         Field 2 length.
          | 
       |
| uint8_t | f3 | 
| 
         Field 3 length.
          | 
       |
| uint8_t | f4 | 
| 
         Field 4 length.
          | 
       |
| uint8_t | f5 | 
| 
         Field 5 length.
          | 
       |
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emdrv/ezradiodrv/plugins/inc/
       
ezradio_transmit_plugin.h