Defines command to be executed using STIG mechanism.
       Definition at line
       
        165
       
       of file
       
        em_qspi.h
       
       .
      
      
       #include <
       
     
        em_qspi.h
       
       >
      
         Data Fields | 
       |
| uint32_t | address | 
| uint8_t | addrSize | 
| uint8_t | cmdOpcode | 
| uint8_t | dummyCycles | 
| bool | modeBitEnable | 
| void * | readBuffer | 
| uint16_t | readDataSize | 
| void * | writeBuffer | 
| uint8_t | writeDataSize | 
Field Documentation
| uint32_t QSPI_StigCmd_TypeDef::address | 
Flash command address.
        Definition at line
        
         179
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| uint8_t QSPI_StigCmd_TypeDef::addrSize | 
Number of Address Bytes.
        Definition at line
        
         171
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| uint8_t QSPI_StigCmd_TypeDef::cmdOpcode | 
| uint8_t QSPI_StigCmd_TypeDef::dummyCycles | 
Number of dummy cycles.
        Definition at line
        
         175
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| bool QSPI_StigCmd_TypeDef::modeBitEnable | 
Mode Bit Configuration register are sent following the address bytes.
        Definition at line
        
         177
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| void* QSPI_StigCmd_TypeDef::readBuffer | 
| uint16_t QSPI_StigCmd_TypeDef::readDataSize | 
Number of Read Data Bytes.
        Definition at line
        
         169
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| void* QSPI_StigCmd_TypeDef::writeBuffer | 
Buffer with data to write.
        Definition at line
        
         183
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| uint8_t QSPI_StigCmd_TypeDef::writeDataSize | 
Number of Write Data Bytes.
        Definition at line
        
         173
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_qspi.h