TFT Initialization structure.
       Definition at line
       
        588
       
       of file
       
        em_ebi.h
       
       .
      
      
       #include <
       
     
        em_ebi.h
       
       >
      
Field Documentation
| uint32_t EBI_TFTInit_TypeDef::addressOffset | 
TFT Frame Buffer address, offset to EBI bank base address.
        Definition at line
        
         632
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_TFTBank_TypeDef EBI_TFTInit_TypeDef::bank | 
External memory bank for driving display.
        Definition at line
        
         590
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_TFTColorSrc_TypeDef EBI_TFTInit_TypeDef::colSrc | 
Color source for masking and alpha blending.
        Definition at line
        
         594
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::csPolarity | 
TFT Polarity for Chip Select (CS) Line.
        Definition at line
        
         606
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::dataenPolarity | 
TFT Polarity for Data Enable (DATAEN) Line.
        Definition at line
        
         610
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::dclkPeriod | 
TFT DCLK period in internal cycles.
        Definition at line
        
         634
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::dclkPolarity | 
TFT Polarity for Data Clock (DCLK) Line.
        Definition at line
        
         608
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_TFTDDMode_TypeDef EBI_TFTInit_TypeDef::driveMode | 
| EBI_TFTFrameBufTrigger_TypeDef EBI_TFTInit_TypeDef::fbTrigger | 
Trigger for updating frame buffer pointer.
        Definition at line
        
         598
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::holdCycles | 
Number of cycles RGB data is held after active edge of DCLK.
        Definition at line
        
         640
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::hPorchBack | 
| int EBI_TFTInit_TypeDef::hPorchFront | 
Horizontal Front Porch Size.
        Definition at line
        
         618
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::hPulseWidth | 
Horizontal Synchronization Pulse Width.
        Definition at line
        
         622
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::hsize | 
| EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::hsyncPolarity | 
TFT Polarity for Horizontal Sync (HSYNC) Line.
        Definition at line
        
         612
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_TFTInterleave_TypeDef EBI_TFTInit_TypeDef::interleave | 
| EBI_TFTMaskBlend_TypeDef EBI_TFTInit_TypeDef::maskBlend | 
Masking and alpha blending mode.
        Definition at line
        
         602
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::setupCycles | 
Number of cycles RGB data is driven before active edge of DCLK.
        Definition at line
        
         638
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| bool EBI_TFTInit_TypeDef::shiftDClk | 
Drive DCLK from negative clock edge of internal clock.
        Definition at line
        
         600
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::startPosition | 
Starting position of External Direct Drive relative to DCLK inactive edge.
        Definition at line
        
         636
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::vPorchBack | 
| int EBI_TFTInit_TypeDef::vPorchFront | 
| int EBI_TFTInit_TypeDef::vPulseWidth | 
Vertical Synchronization Pulse Width.
        Definition at line
        
         630
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| int EBI_TFTInit_TypeDef::vsize | 
| EBI_Polarity_TypeDef EBI_TFTInit_TypeDef::vsyncPolarity | 
TFT Polarity for Vertical Sync (VSYNC) Line.
        Definition at line
        
         614
        
        of file
        
         em_ebi.h
        
        .
       
Referenced by EBI_TFTInit() .
| EBI_TFTWidth_TypeDef EBI_TFTInit_TypeDef::width | 
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_ebi.h