USB_ConfigurationDescriptor_TypeDef Struct Reference
USB Configuration Descriptor.
       Definition at line
       
        426
       
       of file
       
        em_usb.h
       
       .
      
      
       #include <
       
     
        em_usb.h
       
       >
      
         Data Fields | 
       |
| uint8_t | bConfigurationValue | 
| uint8_t | bDescriptorType | 
| uint8_t | bLength | 
| uint8_t | bmAttributes | 
| uint8_t | bMaxPower | 
| uint8_t | bNumInterfaces | 
| uint8_t | iConfiguration | 
| uint16_t | wTotalLength | 
Field Documentation
| uint8_t USB_ConfigurationDescriptor_TypeDef::bConfigurationValue | 
Value to use as an argument to the SetConfiguration request to select this configuration.
        Definition at line
        
         436
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() .
| uint8_t USB_ConfigurationDescriptor_TypeDef::bDescriptorType | 
Constant CONFIGURATION Descriptor Type
        Definition at line
        
         428
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() .
| uint8_t USB_ConfigurationDescriptor_TypeDef::bLength | 
Size of this descriptor in bytes
        Definition at line
        
         427
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() .
| uint8_t USB_ConfigurationDescriptor_TypeDef::bmAttributes | 
        Configuration characteristics.
        
        D7: Reserved (set to one)
        
        D6: Self-powered
        
        D5: Remote Wakeup
        
        D4...0: Reserved (reset to zero)
       
        Definition at line
        
         441
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() .
| uint8_t USB_ConfigurationDescriptor_TypeDef::bMaxPower | 
Maximum power consumption of the USB device, unit is 2mA per LSB
        Definition at line
        
         446
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() .
| uint8_t USB_ConfigurationDescriptor_TypeDef::bNumInterfaces | 
Number of interfaces supported by this configuration
        Definition at line
        
         434
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() .
| uint8_t USB_ConfigurationDescriptor_TypeDef::iConfiguration | 
Index of string descriptor describing this configuration.
        Definition at line
        
         439
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() .
| uint16_t USB_ConfigurationDescriptor_TypeDef::wTotalLength | 
Total length of data returned for this configuration. Includes the combined length of all descriptors (configuration, interface, endpoint, and class- or vendor-specific) returned for this configuration.
        Definition at line
        
         429
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_PrintConfigurationDescriptor() , and USBH_QueryDeviceB() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/middleware/usb_gecko/inc/
       
em_usb.h