USBH_Init_TypeDef Struct Reference
USB Host stack initialization structure.
This structure is passed to USBH_Init() when starting up the device. Max accumulated FIFO size is 2K bytes.
       Definition at line
       
        881
       
       of file
       
        em_usb.h
       
       .
      
      
       #include <
       
     
        em_usb.h
       
       >
      
         Data Fields | 
       |
| uint32_t | nptxFifoSize | 
| uint32_t | ptxFifoSize | 
| uint32_t | reserved | 
| uint32_t | rxFifoSize | 
Field Documentation
| uint32_t USBH_Init_TypeDef::nptxFifoSize | 
Number of FIFO bytes set aside for OUT CTRL/BULK endoints.
        Definition at line
        
         883
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_Init() .
| uint32_t USBH_Init_TypeDef::ptxFifoSize | 
Number of FIFO bytes set aside for OUT INTR/ISO endoints.
        Definition at line
        
         884
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_Init() .
| uint32_t USBH_Init_TypeDef::reserved | 
Reserved for future use.
        Definition at line
        
         885
        
        of file
        
         em_usb.h
        
        .
       
| uint32_t USBH_Init_TypeDef::rxFifoSize | 
Number of FIFO bytes set aside for IN endpoints.
        Definition at line
        
         882
        
        of file
        
         em_usb.h
        
        .
       
Referenced by USBH_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/middleware/usb_gecko/inc/
       
em_usb.h