CAN initialization structure.
       Definition at line
       
        154
       
       of file
       
        em_can.h
       
       .
      
      
       #include <
       
     
        em_can.h
       
       >
      
         Data Fields | 
       |
| uint32_t | bitrate | 
| bool | enable | 
| uint8_t | phaseBufferSegment1 | 
| uint8_t | phaseBufferSegment2 | 
| uint8_t | propagationTimeSegment | 
| bool | resetMessages | 
| uint8_t | synchronisationJumpWidth | 
Field Documentation
| uint32_t CAN_Init_TypeDef::bitrate | 
| bool CAN_Init_TypeDef::enable | 
True to set the CAN Device in normal mode after initialization.
        Definition at line
        
         156
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_Init() .
| uint8_t CAN_Init_TypeDef::phaseBufferSegment1 | 
Default Phase Buffer Segment 1.
        Definition at line
        
         168
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_Init() .
| uint8_t CAN_Init_TypeDef::phaseBufferSegment2 | 
Default Phase Buffer Segment 2.
        Definition at line
        
         171
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_Init() .
| uint8_t CAN_Init_TypeDef::propagationTimeSegment | 
Default Propagation Time Segment.
        Definition at line
        
         165
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_Init() .
| bool CAN_Init_TypeDef::resetMessages | 
True to reset messages during initialization.
        Definition at line
        
         159
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_Init() .
| uint8_t CAN_Init_TypeDef::synchronisationJumpWidth | 
Default Synchronisation Jump Width.
        Definition at line
        
         174
        
        of file
        
         em_can.h
        
        .
       
Referenced by CAN_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_can.h