QSPI Device Delay Configuration Structure.
       Definition at line
       
        148
       
       of file
       
        em_qspi.h
       
       .
      
      
       #include <
       
     
        em_qspi.h
       
       >
      
         Data Fields | 
       |
| uint8_t | deassert | 
| uint8_t | deviceSwitch | 
| uint8_t | firstBit | 
| uint8_t | lastBit | 
Field Documentation
| uint8_t QSPI_DelayConfig_TypeDef::deassert | 
The minimal delay to keep the chip select line de-asserted between two transactions.
        Definition at line
        
         151
        
        of file
        
         em_qspi.h
        
        .
       
| uint8_t QSPI_DelayConfig_TypeDef::deviceSwitch | 
Delay between one chip select being de-activated and the activation of another.
        Definition at line
        
         155
        
        of file
        
         em_qspi.h
        
        .
       
| uint8_t QSPI_DelayConfig_TypeDef::firstBit | 
Delay chip select assert and first bit in a transaction.
        Definition at line
        
         161
        
        of file
        
         em_qspi.h
        
        .
       
| uint8_t QSPI_DelayConfig_TypeDef::lastBit | 
Delay between last bit and chip select de-assert.
        Definition at line
        
         158
        
        of file
        
         em_qspi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_qspi.h