This module includes functions that control DNS communication.

Classes

struct otDnsQuery
This structure implements DNS Query parameters.

Macros

#define OT_DNS_MAX_HOSTNAME_LENGTH 62
Maximum allowed hostname length (maximum label size - 1 for compression).
#define OT_DNS_DEFAULT_SERVER_IP "2001:4860:4860::8888"
Defines default DNS Server address - Google DNS.
#define OT_DNS_DEFAULT_SERVER_PORT 53
Defines default DNS Server port.

Typedefs

typedef struct otDnsQuery otDnsQuery
This structure implements DNS Query parameters.
typedef void(* otDnsResponseHandler ) (void *aContext, const char *aHostname, const otIp6Address *aAddress, uint32_t aTtl, otError aResult)
This function pointer is called when a DNS response is received.

Functions

otError otDnsClientQuery ( otInstance *aInstance, const otDnsQuery *aQuery, otDnsResponseHandler aHandler, void *aContext)
This function sends a DNS query for AAAA (IPv6) record.

Detailed Description

This module includes functions that control DNS communication.

Typedef Documentation

◆ otDnsResponseHandler

typedef void(* otDnsResponseHandler) (void *aContext, const char *aHostname, const otIp6Address *aAddress, uint32_t aTtl, otError aResult)

This function pointer is called when a DNS response is received.

Parameters
[in] aContext A pointer to application-specific context.
[in] aHostname Identifies hostname related with DNS response.
[in] aAddress A pointer to the IPv6 address received in DNS response. May be null.
[in] aTtl Specifies the maximum time in seconds that the resource record may be cached.
[in] aResult A result of the DNS transaction.
Return values
OT_ERROR_NONE A response was received successfully and IPv6 address is provided in aAddress .
OT_ERROR_ABORT A DNS transaction was aborted by stack.
OT_ERROR_RESPONSE_TIMEOUT No DNS response has been received within timeout.
OT_ERROR_NOT_FOUND A response was received but no IPv6 address has been found.
OT_ERROR_FAILED A response was received but status code is different than success.

Function Documentation

◆ otDnsClientQuery()

otError otDnsClientQuery ( otInstance * aInstance,
const otDnsQuery * aQuery,
otDnsResponseHandler aHandler,
void * aContext
)

This function sends a DNS query for AAAA (IPv6) record.

This function is available only if feature OPENTHREAD_CONFIG_DNS_CLIENT_ENABLE is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aQuery A pointer to specify DNS query parameters.
[in] aHandler A function pointer that shall be called on response reception or time-out.
[in] aContext A pointer to arbitrary context information.