This module includes the platform abstraction for the message pool.

Functions

void otPlatMessagePoolInit ( otInstance *aInstance, uint16_t aMinNumFreeBuffers, size_t aBufferSize)
Initialize the platform implemented message pool.
otMessage * otPlatMessagePoolNew ( otInstance *aInstance)
Allocate a buffer from the platform managed buffer pool.
void otPlatMessagePoolFree ( otInstance *aInstance, otMessage *aBuffer)
This function is used to free a Buffer back to the platform managed buffer pool.
uint16_t otPlatMessagePoolNumFreeBuffers ( otInstance *aInstance)
Get the number of free buffers.

Detailed Description

This module includes the platform abstraction for the message pool.

Function Documentation

◆ otPlatMessagePoolFree()

void otPlatMessagePoolFree ( otInstance * aInstance,
otMessage * aBuffer
)

This function is used to free a Buffer back to the platform managed buffer pool.

Parameters
[in] aInstance A pointer to the OpenThread instance.
[in] aBuffer The Buffer to free.

◆ otPlatMessagePoolInit()

void otPlatMessagePoolInit ( otInstance * aInstance,
uint16_t aMinNumFreeBuffers,
size_t aBufferSize
)

Initialize the platform implemented message pool.

Parameters
[in] aInstance A pointer to the OpenThread instance.
[in] aMinNumFreeBuffers An uint16 containing the minimum number of free buffers desired by OpenThread.
[in] aBufferSize The size in bytes of a Buffer object.

◆ otPlatMessagePoolNew()

otMessage * otPlatMessagePoolNew ( otInstance * aInstance )

Allocate a buffer from the platform managed buffer pool.

Parameters
[in] aInstance A pointer to the OpenThread instance.
Returns
A pointer to the Buffer or NULL if no Buffers are available.

◆ otPlatMessagePoolNumFreeBuffers()

uint16_t otPlatMessagePoolNumFreeBuffers ( otInstance * aInstance )

Get the number of free buffers.

Parameters
[in] aInstance A pointer to the OpenThread instance.
Returns
The number of buffers currently free and available to OpenThread.