otRadioIeInfo Struct Reference
This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame.
#include <
include/openthread/platform/radio.h
>
Public Attributes |
|
int64_t | mNetworkTimeOffset |
The time offset to the Thread network time.
|
|
uint8_t | mTimeIeOffset |
The Time IE offset from the start of PSDU.
|
|
uint8_t | mTimeSyncSeq |
The Time sync sequence.
|
This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame.
The documentation for this struct was generated from the following file:
-
include/openthread/platform/
radio.h