otActiveScanResult Struct Reference

This structure represents a received IEEE 802.15.4 Beacon.

#include < include/openthread/link.h >

Public Attributes

otExtAddress mExtAddress
IEEE 802.15.4 Extended Address.
otNetworkName mNetworkName
Thread Network Name.
otExtendedPanId mExtendedPanId
Thread Extended PAN ID.
otSteeringData mSteeringData
Steering Data.
uint16_t mPanId
IEEE 802.15.4 PAN ID.
uint16_t mJoinerUdpPort
Joiner UDP Port.
uint8_t mChannel
IEEE 802.15.4 Channel.
int8_t mRssi
RSSI (dBm)
uint8_t mLqi
LQI.
unsigned int mVersion : 4
Version.
bool mIsNative : 1
Native Commissioner flag.
bool mIsJoinable : 1
Joining Permitted flag.

This structure represents a received IEEE 802.15.4 Beacon.


The documentation for this struct was generated from the following file:
  • include/openthread/ link.h