otNetworkDiagRoute Struct Reference

This structure represents a Network Diagnostic Route TLV value.

#include < include/openthread/netdiag.h >

Public Attributes

uint8_t mIdSequence
The sequence number associated with the set of Router ID assignments in mRouteData .
uint8_t mRouteCount
Number of elements in mRouteData .
otNetworkDiagRouteData mRouteData [ OT_NETWORK_MAX_ROUTER_ID +1]
Link Quality and Routing Cost data.

This structure represents a Network Diagnostic Route TLV value.


The documentation for this struct was generated from the following file:
  • include/openthread/ netdiag.h