otChildInfo Struct Reference
This structure holds diagnostic information for a Thread Child.
#include <
include/openthread/thread_ftd.h
>
Public Attributes | |
otExtAddress | mExtAddress |
IEEE 802.15.4 Extended Address. | |
uint32_t | mTimeout |
Timeout. | |
uint32_t | mAge |
Time last heard. | |
uint16_t | mRloc16 |
RLOC16. | |
uint16_t | mChildId |
Child ID. | |
uint8_t | mNetworkDataVersion |
Network Data Version. | |
uint8_t | mLinkQualityIn |
Link Quality In. | |
int8_t | mAverageRssi |
Average RSSI. | |
int8_t | mLastRssi |
Last observed RSSI. | |
uint16_t | mFrameErrorRate |
Frame error rate (0xffff->100%). Requires error tracking feature. | |
uint16_t | mMessageErrorRate |
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature. | |
bool | mRxOnWhenIdle: 1 |
rx-on-when-idle | |
bool | mFullThreadDevice: 1 |
Full Thread Device. | |
bool | mFullNetworkData: 1 |
Full Network Data. | |
bool | mIsStateRestoring: 1 |
Is in restoring state. |
This structure holds diagnostic information for a Thread Child.
The documentation for this struct was generated from the following file:
- include/openthread/
thread_ftd.h