otCacheEntryIterator Struct Reference

This type represents an iterator used for iterating through the EID cache table entries.

#include < include/openthread/thread_ftd.h >

Public Attributes

const void * mData [2]
Opaque data used by the core implementation. Should not be changed by user.

This type represents an iterator used for iterating through the EID cache table entries.

To initialize the iterator and start from the first entry in the cache table, set all its fields in the structure to zero (e.g., memset the iterator to zero).


The documentation for this struct was generated from the following file:
  • include/openthread/ thread_ftd.h