otRouterInfo Struct Reference

This structure holds diagnostic information for a Thread Router.

#include < include/openthread/thread.h >

Public Attributes

otExtAddress mExtAddress
IEEE 802.15.4 Extended Address.
uint16_t mRloc16
RLOC16.
uint8_t mRouterId
Router ID.
uint8_t mNextHop
Next hop to router.
uint8_t mPathCost
Path cost to router.
uint8_t mLinkQualityIn
Link Quality In.
uint8_t mLinkQualityOut
Link Quality Out.
uint8_t mAge
Time last heard.
bool mAllocated : 1
Router ID allocated or not.
bool mLinkEstablished : 1
Link established with Router ID or not.

This structure holds diagnostic information for a Thread Router.


The documentation for this struct was generated from the following file:
  • include/openthread/ thread.h