otLinkModeConfig Struct Reference

This structure represents an MLE Link Mode configuration.

#include < include/openthread/thread.h >

Public Attributes

bool mRxOnWhenIdle : 1
1, if the sender has its receiver on when not transmitting. 0, otherwise.
bool mDeviceType : 1
1, if the sender is an FTD. 0, otherwise.
bool mNetworkData : 1
1, if the sender requires the full Network Data. 0, otherwise.

This structure represents an MLE Link Mode configuration.


The documentation for this struct was generated from the following file:
  • include/openthread/ thread.h