otCommissioningDataset Struct Reference
This structure represents a Commissioning Dataset.
#include <
include/openthread/commissioner.h
>
Public Attributes |
|
uint16_t | mLocator |
Border Router RLOC16.
|
|
uint16_t | mSessionId |
Commissioner Session Id.
|
|
otSteeringData | mSteeringData |
Steering Data.
|
|
uint16_t | mJoinerUdpPort |
Joiner UDP Port.
|
|
bool | mIsLocatorSet : 1 |
TRUE if Border Router RLOC16 is set, FALSE otherwise.
|
|
bool | mIsSessionIdSet : 1 |
TRUE if Commissioner Session Id is set, FALSE otherwise.
|
|
bool | mIsSteeringDataSet : 1 |
TRUE if Steering Data is set, FALSE otherwise.
|
|
bool | mIsJoinerUdpPortSet : 1 |
TRUE if Joiner UDP Port is set, FALSE otherwise.
|
This structure represents a Commissioning Dataset.
The documentation for this struct was generated from the following file:
-
include/openthread/
commissioner.h