Jam Detection

This module includes functions for signal jamming detection feature.

Typedefs

typedef void(* otJamDetectionCallback ) (bool aJamState, void *aContext)
This function pointer is called if signal jam detection is enabled and a jam is detected.

Functions

otError otJamDetectionSetRssiThreshold ( otInstance *aInstance, int8_t aRssiThreshold)
Set the Jam Detection RSSI Threshold (in dBm).
int8_t otJamDetectionGetRssiThreshold ( otInstance *aInstance)
Get the Jam Detection RSSI Threshold (in dBm).
otError otJamDetectionSetWindow ( otInstance *aInstance, uint8_t aWindow)
Set the Jam Detection Detection Window (in seconds).
uint8_t otJamDetectionGetWindow ( otInstance *aInstance)
Get the Jam Detection Detection Window (in seconds).
otError otJamDetectionSetBusyPeriod ( otInstance *aInstance, uint8_t aBusyPeriod)
Set the Jam Detection Busy Period (in seconds).
uint8_t otJamDetectionGetBusyPeriod ( otInstance *aInstance)
Get the Jam Detection Busy Period (in seconds)
otError otJamDetectionStart ( otInstance *aInstance, otJamDetectionCallback aCallback, void *aContext)
Start the jamming detection.
otError otJamDetectionStop ( otInstance *aInstance)
Stop the jamming detection.
bool otJamDetectionIsEnabled ( otInstance *aInstance)
Get the Jam Detection Status (enabled/disabled)
bool otJamDetectionGetState ( otInstance *aInstance)
Get the Jam Detection State.
uint64_t otJamDetectionGetHistoryBitmap ( otInstance *aInstance)
Get the current history bitmap.

Detailed Description

This module includes functions for signal jamming detection feature.

The functions in this module are available when jam-detection feature ( OPENTHREAD_CONFIG_JAM_DETECTION_ENABLE ) is enabled.

Typedef Documentation

◆ otJamDetectionCallback

typedef void(* otJamDetectionCallback) (bool aJamState, void *aContext)

This function pointer is called if signal jam detection is enabled and a jam is detected.

Parameters
[in] aJamState Current jam state ( true if jam is detected, false otherwise).
[in] aContext A pointer to application-specific context.

Function Documentation

◆ otJamDetectionGetBusyPeriod()

uint8_t otJamDetectionGetBusyPeriod ( otInstance * aInstance )

Get the Jam Detection Busy Period (in seconds)

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Jam Detection Busy Period.

◆ otJamDetectionGetHistoryBitmap()

uint64_t otJamDetectionGetHistoryBitmap ( otInstance * aInstance )

Get the current history bitmap.

This value provides information about current state of jamming detection module for monitoring/debugging purpose. It returns a 64-bit value where each bit corresponds to one second interval starting with bit 0 for the most recent interval and bit 63 for the oldest intervals (63 sec earlier). The bit is set to 1 if the jamming detection module observed/detected high signal level during the corresponding one second interval.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The current history bitmap.

◆ otJamDetectionGetRssiThreshold()

int8_t otJamDetectionGetRssiThreshold ( otInstance * aInstance )

Get the Jam Detection RSSI Threshold (in dBm).

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Jam Detection RSSI Threshold.

◆ otJamDetectionGetState()

bool otJamDetectionGetState ( otInstance * aInstance )

Get the Jam Detection State.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Jam Detection state ( true jam is detected, `false' otherwise).

◆ otJamDetectionGetWindow()

uint8_t otJamDetectionGetWindow ( otInstance * aInstance )

Get the Jam Detection Detection Window (in seconds).

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Jam Detection Window.

◆ otJamDetectionIsEnabled()

bool otJamDetectionIsEnabled ( otInstance * aInstance )

Get the Jam Detection Status (enabled/disabled)

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Jam Detection status (true if enabled, false otherwise).

◆ otJamDetectionSetBusyPeriod()

otError otJamDetectionSetBusyPeriod ( otInstance * aInstance,
uint8_t aBusyPeriod
)

Set the Jam Detection Busy Period (in seconds).

The number of aggregate seconds within the detection window where the RSSI must be above threshold to trigger detection.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aBusyPeriod The Jam Detection busy period (should be non-zero and less than or equal to Jam Detection Window)
Return values
OT_ERROR_NONE Successfully set the window.
OT_ERROR_INVALID_ARGS The given input is not within the valid range.

◆ otJamDetectionSetRssiThreshold()

otError otJamDetectionSetRssiThreshold ( otInstance * aInstance,
int8_t aRssiThreshold
)

Set the Jam Detection RSSI Threshold (in dBm).

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aRssiThreshold The RSSI threshold.
Return values
OT_ERROR_NONE Successfully set the threshold.

◆ otJamDetectionSetWindow()

otError otJamDetectionSetWindow ( otInstance * aInstance,
uint8_t aWindow
)

Set the Jam Detection Detection Window (in seconds).

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aWindow The Jam Detection window (valid range is 1 to 63)
Return values
OT_ERROR_NONE Successfully set the window.
OT_ERROR_INVALID_ARGS The given input parameter not within valid range (1-63)

◆ otJamDetectionStart()

otError otJamDetectionStart ( otInstance * aInstance,
otJamDetectionCallback aCallback,
void * aContext
)

Start the jamming detection.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aCallback A pointer to a function called to notify of jamming state change.
[in] aContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Successfully started the jamming detection.
OT_ERROR_ALREADY Jam detection has been started before.

◆ otJamDetectionStop()

otError otJamDetectionStop ( otInstance * aInstance )

Stop the jamming detection.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE Successfully stopped the jamming detection.
OT_ERROR_ALREADY Jam detection is already stopped.