This module includes functions that control UDP communication.

Classes

struct otUdpReceiver
This structure represents a UDP receiver.
struct otUdpSocket
This structure represents a UDP socket.

Typedefs

typedef bool(* otUdpHandler ) (void *aContext, const otMessage *aMessage, const otMessageInfo *aMessageInfo)
This callback allows OpenThread to provide specific handlers for certain UDP messages.
typedef struct otUdpReceiver otUdpReceiver
This structure represents a UDP receiver.
typedef void(* otUdpReceive ) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo)
This callback allows OpenThread to inform the application of a received UDP message.
typedef struct otUdpSocket otUdpSocket
This structure represents a UDP socket.

Functions

otError otUdpAddReceiver ( otInstance *aInstance, otUdpReceiver *aUdpReceiver)
This function adds a UDP receiver.
otError otUdpRemoveReceiver ( otInstance *aInstance, otUdpReceiver *aUdpReceiver)
This function removes a UDP receiver.
otError otUdpSendDatagram ( otInstance *aInstance, otMessage *aMessage, otMessageInfo *aMessageInfo)
This function sends a UDP message without socket.
otMessage * otUdpNewMessage ( otInstance *aInstance, const otMessageSettings *aSettings)
Allocate a new message buffer for sending a UDP message.
otError otUdpOpen ( otInstance *aInstance, otUdpSocket *aSocket, otUdpReceive aCallback, void *aContext)
Open a UDP/IPv6 socket.
otError otUdpClose ( otInstance *aInstance, otUdpSocket *aSocket)
Close a UDP/IPv6 socket.
otError otUdpBind ( otInstance *aInstance, otUdpSocket *aSocket, const otSockAddr *aSockName)
Bind a UDP/IPv6 socket.
otError otUdpConnect ( otInstance *aInstance, otUdpSocket *aSocket, const otSockAddr *aSockName)
Connect a UDP/IPv6 socket.
otError otUdpSend ( otInstance *aInstance, otUdpSocket *aSocket, otMessage *aMessage, const otMessageInfo *aMessageInfo)
Send a UDP/IPv6 message.
otUdpSocket * otUdpGetSockets ( otInstance *aInstance)
This function gets the head of linked list of UDP Sockets.

Detailed Description

This module includes functions that control UDP communication.

Typedef Documentation

◆ otUdpHandler

typedef bool(* otUdpHandler) (void *aContext, const otMessage *aMessage, const otMessageInfo *aMessageInfo)

This callback allows OpenThread to provide specific handlers for certain UDP messages.

Return values
true The message is handled by this receiver and should not be further processed.
false The message is not handled by this receiver.

Function Documentation

◆ otUdpAddReceiver()

otError otUdpAddReceiver ( otInstance * aInstance,
otUdpReceiver * aUdpReceiver
)

This function adds a UDP receiver.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aUdpReceiver A pointer to the UDP receiver.
Return values
OT_ERROR_NONE The receiver is successfully added.
OT_ERROR_ALREADY The UDP receiver was already added.

◆ otUdpBind()

otError otUdpBind ( otInstance * aInstance,
otUdpSocket * aSocket,
const otSockAddr * aSockName
)

Bind a UDP/IPv6 socket.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSocket A pointer to a UDP socket structure.
[in] aSockName A pointer to an IPv6 socket address structure.
Return values
OT_ERROR_NONE Bind operation was successful.
OT_ERROR_FAILED Failed to bind UDP socket.

◆ otUdpClose()

otError otUdpClose ( otInstance * aInstance,
otUdpSocket * aSocket
)

Close a UDP/IPv6 socket.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSocket A pointer to a UDP socket structure.
Return values
OT_ERROR_NONE Successfully closed the socket.
OT_ERROR_FAILED Failed to close UDP Socket.

◆ otUdpConnect()

otError otUdpConnect ( otInstance * aInstance,
otUdpSocket * aSocket,
const otSockAddr * aSockName
)

Connect a UDP/IPv6 socket.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSocket A pointer to a UDP socket structure.
[in] aSockName A pointer to an IPv6 socket address structure.
Return values
OT_ERROR_NONE Connect operation was successful.
OT_ERROR_FAILED Failed to connect UDP socket.

◆ otUdpGetSockets()

otUdpSocket * otUdpGetSockets ( otInstance * aInstance )

This function gets the head of linked list of UDP Sockets.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the head of UDP Socket linked list.

◆ otUdpNewMessage()

otMessage * otUdpNewMessage ( otInstance * aInstance,
const otMessageSettings * aSettings
)

Allocate a new message buffer for sending a UDP message.

Note
If aSettings is 'NULL', the link layer security is enabled and the message priority is set to OT_MESSAGE_PRIORITY_NORMAL by default.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSettings A pointer to the message settings or NULL to use default settings.
Returns
A pointer to the message buffer or NULL if no message buffers are available or parameters are invalid.
See also
otMessageFree

◆ otUdpOpen()

otError otUdpOpen ( otInstance * aInstance,
otUdpSocket * aSocket,
otUdpReceive aCallback,
void * aContext
)

Open a UDP/IPv6 socket.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSocket A pointer to a UDP socket structure.
[in] aCallback A pointer to the application callback function.
[in] aContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Successfully opened the socket.
OT_ERROR_FAILED Failed to open the socket.

◆ otUdpRemoveReceiver()

otError otUdpRemoveReceiver ( otInstance * aInstance,
otUdpReceiver * aUdpReceiver
)

This function removes a UDP receiver.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aUdpReceiver A pointer to the UDP receiver.
Return values
OT_ERROR_NONE The receiver is successfully removed.
OT_ERROR_NOT_FOUND The UDP receiver was not added.

◆ otUdpSend()

otError otUdpSend ( otInstance * aInstance,
otUdpSocket * aSocket,
otMessage * aMessage,
const otMessageInfo * aMessageInfo
)

Send a UDP/IPv6 message.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSocket A pointer to a UDP socket structure.
[in] aMessage A pointer to a message buffer.
[in] aMessageInfo A pointer to a message info structure.

If the return value is OT_ERROR_NONE, OpenThread takes ownership of aMessage , and the caller should no longer reference aMessage . If the return value is not OT_ERROR_NONE, the caller retains ownership of aMessage , including freeing aMessage if the message buffer is no longer needed.

Return values
OT_ERROR_NONE The message is successfully scheduled for sending.
OT_ERROR_INVALID_ARGS Invalid arguments are given.
OT_ERROR_NO_BUFS Insufficient available buffer to add the UDP and IPv6 headers.

◆ otUdpSendDatagram()

otError otUdpSendDatagram ( otInstance * aInstance,
otMessage * aMessage,
otMessageInfo * aMessageInfo
)

This function sends a UDP message without socket.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to a message without UDP header.
[in] aMessageInfo A pointer to a message info associated with aMessage .
Return values
OT_ERROR_NONE Successfully enqueued the message into an output interface.
OT_ERROR_NO_BUFS Insufficient available buffer to add the IPv6 headers.