This module includes OpenThread logging related definitions.

Functions

otLogLevel otLoggingGetLevel (void)
This function returns the current log level.
otError otLoggingSetLevel ( otLogLevel aLogLevel)
This function sets the log level.

Detailed Description

This module includes OpenThread logging related definitions.

Function Documentation

◆ otLoggingGetLevel()

otLogLevel otLoggingGetLevel ( void )

This function returns the current log level.

If dynamic log level feature OPENTHREAD_CONFIG_LOG_LEVEL_DYNAMIC_ENABLE is enabled, this function returns the currently set dynamic log level. Otherwise, this function returns the build-time configured log level.

Returns
The log level.

◆ otLoggingSetLevel()

otError otLoggingSetLevel ( otLogLevel aLogLevel )

This function sets the log level.

Note
This function requires OPENTHREAD_CONFIG_LOG_LEVEL_DYNAMIC_ENABLE=1 .
Parameters
[in] aLogLevel The log level.
Return values
OT_ERROR_NONE Successfully updated log level.
OT_ERROR_INVALID_ARGS Log level value is invalid.