otCacheEntryInfo Struct Reference

This structure represents an EID cache entry.

#include < include/openthread/thread_ftd.h >

Public Attributes

otIp6Address mTarget
Target EID.
otShortAddress mRloc16
RLOC16.
otCacheEntryState mState
Entry state.
bool mCanEvict : 1
Indicates whether the entry can be evicted.
bool mValidLastTrans : 1
Indicates whether last transaction time and ML-EID are valid.
uint32_t mLastTransTime
Last transaction time (applicable in cached state).
otIp6Address mMeshLocalEid
Mesh Local EID (applicable if entry in cached state).
uint16_t mTimeout
Timeout in seconds (applicable if in snooped/query/retry-query states).
uint16_t mRetryDelay
Retry delay in seconds (applicable if in query-retry state).

This structure represents an EID cache entry.


The documentation for this struct was generated from the following file:
  • include/openthread/ thread_ftd.h