otExtAddress Struct Reference

This structure represents the IEEE 802.15.4 Extended Address.

#include < include/openthread/platform/radio.h >

Public Attributes

uint8_t m8 [ OT_EXT_ADDRESS_SIZE ]
IEEE 802.15.4 Extended Address bytes.

This structure represents the IEEE 802.15.4 Extended Address.


The documentation for this struct was generated from the following file:
  • include/openthread/platform/ radio.h