This module includes functions that control SNTP communication.

Classes

struct otSntpQuery
This structure implements SNTP Query parameters.

Macros

#define OT_SNTP_DEFAULT_SERVER_IP "2001:4860:4806:8::"
Defines default SNTP Server address - Google NTP Server.
#define OT_SNTP_DEFAULT_SERVER_PORT 123
Defines default SNTP Server port.

Typedefs

typedef struct otSntpQuery otSntpQuery
This structure implements SNTP Query parameters.
typedef void(* otSntpResponseHandler ) (void *aContext, uint64_t aTime, otError aResult)
This function pointer is called when a SNTP response is received.

Functions

otError otSntpClientQuery ( otInstance *aInstance, const otSntpQuery *aQuery, otSntpResponseHandler aHandler, void *aContext)
This function sends a SNTP query.
void otSntpClientSetUnixEra ( otInstance *aInstance, uint32_t aUnixEra)
This function sets the unix era number.

Detailed Description

This module includes functions that control SNTP communication.

Typedef Documentation

◆ otSntpResponseHandler

typedef void(* otSntpResponseHandler) (void *aContext, uint64_t aTime, otError aResult)

This function pointer is called when a SNTP response is received.

Parameters
[in] aContext A pointer to application-specific context.
[in] aTime Specifies the time at the server when the response left for the client, in UNIX time.
[in] aResult A result of the SNTP transaction.
Return values
OT_ERROR_NONE A response was received successfully and time is provided in aTime .
OT_ERROR_ABORT A SNTP transaction was aborted by stack.
OT_ERROR_BUSY The Kiss-o'-death packet has been received.
OT_ERROR_RESPONSE_TIMEOUT No SNTP response has been received within timeout.
OT_ERROR_FAILED A response was received but contains incorrect data.

Function Documentation

◆ otSntpClientQuery()

otError otSntpClientQuery ( otInstance * aInstance,
const otSntpQuery * aQuery,
otSntpResponseHandler aHandler,
void * aContext
)

This function sends a SNTP query.

This function is available only if feature OPENTHREAD_CONFIG_SNTP_CLIENT_ENABLE_CLIENT is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aQuery A pointer to specify SNTP query parameters.
[in] aHandler A function pointer that shall be called on response reception or time-out.
[in] aContext A pointer to arbitrary context information.

◆ otSntpClientSetUnixEra()

void otSntpClientSetUnixEra ( otInstance * aInstance,
uint32_t aUnixEra
)

This function sets the unix era number.

The default value of unix era is set to 0. The subsequent eras start after year 2106.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aUnixEra Unix era number.