This structure represents link-specific information for messages received from the Thread radio.
#include <
include/openthread/link.h
>
Public Attributes |
|
| uint16_t | mPanId |
|
Source PAN ID.
|
|
| uint8_t | mChannel |
|
802.15.4 Channel
|
|
| int8_t | mRss |
|
Received Signal Strength in dBm.
|
|
| uint8_t | mLqi |
|
Link Quality Indicator for a received message.
|
|
| bool | mLinkSecurity |
|
Indicates whether or not link security is enabled.
|
|
| uint8_t | mTimeSyncSeq |
|
The time sync sequence.
|
|
| int64_t | mNetworkTimeOffset |
|
The time offset to the Thread network time, in microseconds.
|
|
This structure represents link-specific information for messages received from the Thread radio.
The documentation for this struct was generated from the following file:
-
include/openthread/
link.h