otBufferInfo Struct Reference

This structure represents the message buffer information.

#include < include/openthread/message.h >

Public Attributes

uint16_t mTotalBuffers
The number of buffers in the pool.
uint16_t mFreeBuffers
The number of free message buffers.
uint16_t m6loSendMessages
The number of messages in the 6lo send queue.
uint16_t m6loSendBuffers
The number of buffers in the 6lo send queue.
uint16_t m6loReassemblyMessages
The number of messages in the 6LoWPAN reassembly queue.
uint16_t m6loReassemblyBuffers
The number of buffers in the 6LoWPAN reassembly queue.
uint16_t mIp6Messages
The number of messages in the IPv6 send queue.
uint16_t mIp6Buffers
The number of buffers in the IPv6 send queue.
uint16_t mMplMessages
The number of messages in the MPL send queue.
uint16_t mMplBuffers
The number of buffers in the MPL send queue.
uint16_t mMleMessages
The number of messages in the MLE send queue.
uint16_t mMleBuffers
The number of buffers in the MLE send queue.
uint16_t mArpMessages
The number of messages in the ARP send queue.
uint16_t mArpBuffers
The number of buffers in the ARP send queue.
uint16_t mCoapMessages
The number of messages in the CoAP send queue.
uint16_t mCoapBuffers
The number of buffers in the CoAP send queue.
uint16_t mCoapSecureMessages
The number of messages in the CoAP secure send queue.
uint16_t mCoapSecureBuffers
The number of buffers in the CoAP secure send queue.
uint16_t mApplicationCoapMessages
The number of messages in the application CoAP send queue.
uint16_t mApplicationCoapBuffers
The number of buffers in the application CoAP send queue.

This structure represents the message buffer information.


The documentation for this struct was generated from the following file:
  • include/openthread/ message.h