otThreadParentResponseInfo Struct Reference

This structure represents the MLE Parent Response data.

#include < include/openthread/thread.h >

Public Attributes

otExtAddress mExtAddr
IEEE 802.15.4 Extended Address of the Parent.
uint16_t mRloc16
Short address of the Parent.
int8_t mRssi
Rssi of the Parent.
int8_t mPriority
Parent priority.
uint8_t mLinkQuality3
Parent Link Quality 3.
uint8_t mLinkQuality2
Parent Link Quality 2.
uint8_t mLinkQuality1
Parent Link Quality 1.
bool mIsAttached
Is the node receiving parent response attached.

This structure represents the MLE Parent Response data.


The documentation for this struct was generated from the following file:
  • include/openthread/ thread.h