Plugin Commands: EZ-Mode Commissioning#

The EZ-Mode Commissioning plugin contributes several commands to the application framework's CLI.

Macros#

#define

plugin ezmode-commissioning client [endpoint:1] [direction:1] [clusterIds:2]

#define

plugin ezmode-commissioning server [endpoint:1] [identifyTimeS:2]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_CLIENT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_CLIENT

plugin ezmode-commissioning client [endpoint:1] [direction:1] [clusterIds:2]

  • Start EZ-Mode client commissioning.

    • endpoint - INT8U - The local endpoint.

    • direction - INT8U - ::EMBER_AF_EZMODE_COMMISSIONING_SERVER_TO_CLIENT or ::EMBER_AF_EZMODE_COMMISSIONING_CLIENT_TO_SERVER.

    • clusterIds - INT16U - A list of cluster ids.


Definition at line 2984 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_SERVER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_SERVER

plugin ezmode-commissioning server [endpoint:1] [identifyTimeS:2]

  • Start EZ-Mode server commissioning.

    • endpoint - INT8U - The local endpoint.

    • identifyTimeS - INT16U - The identify time in seconds.


Definition at line 2991 of file ./app/framework/test/headers/cli.doc