Plugin Commands: Calendar Client#

The Calendar Client plugin contributes several commands to the application framework's CLI. These commands are used for interacting with calendars.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_CLEAR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_CLEAR

plugin calendar-client clear [endpoint:1]

  • Clear the calendars.

    • endpoint - INT8U - The endpoint.


Definition at line 1719 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CALENDAR_CLIENT_PLUGIN_CALENDAR_CLIENT_PRINT

plugin calendar-client print [endpoint:1]

  • Print the calendars.

    • endpoint - INT8U - The endpoint.


Definition at line 1725 of file ./app/framework/test/headers/cli.doc