Plugin Commands: Device Table#

The device table plugin demonstrates tracking devices as they join the

gateway's ZigBee network.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_CLEAR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_CLEAR

plugin device-table clear

  • Clear the device table


Definition at line 2828 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_DISC#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_DISC

plugin device-table disc [nodeId:2]

  • Force a (re)discovery of the device based on the node ID.

    • nodeId - INT16U - Node ID to discover.


Definition at line 2834 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_IREMOVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_IREMOVE

plugin device-table iremove [index:2]

  • Remove device from device table.

    • index - INT16U - Device table index.


Definition at line 2840 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_IREPAIR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_IREPAIR

plugin device-table irepair [index:2]

  • Kick off device route repair.

    • index - INT16U - Device table index.


Definition at line 2846 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_ISEND#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_ISEND

plugin device-table isend [index:2]

  • Send to device in device table.

    • index - INT16U - Device table index.


Definition at line 2852 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_LEAVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_LEAVE

plugin device-table leave [eui64:8]

  • Remove device from device table.

    • eui64 - IEEE_ADDRESS - EUI64 of device.


Definition at line 2858 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_LOAD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_LOAD

plugin device-table load

  • Load the file.


Definition at line 2863 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_PRINT

plugin device-table print

  • Print the device table.


Definition at line 2868 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_REMOVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_REMOVE

plugin device-table remove [eui64:8]

  • Remove device from device table.

    • eui64 - IEEE_ADDRESS - EUI64 of device.


Definition at line 2874 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_REPAIR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_REPAIR

plugin device-table repair [eui64:8]

  • Kick off device route repair.

    • eui64 - IEEE_ADDRESS - EUI64 of device.


Definition at line 2880 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_SAVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_SAVE

plugin device-table save

  • Save the file.


Definition at line 2885 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_SEND#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DEVICE_TABLE_PLUGIN_DEVICE_TABLE_SEND

plugin device-table send [eui64:8] [endpoint:1]

  • Send to device in device table.

    • eui64 - IEEE_ADDRESS - EUI64 of device.

    • endpoint - INT8U - Endpoint of device.


Definition at line 2892 of file ./app/framework/test/headers/cli.doc