Plugin Commands: Demand Response and Load Control#

The drlc plugin contributes CLI commands to the application framework to be used for constructing demand response load control commands.

Macros#

#define
#define

plugin drlc opt in [endpoint:1] [eventId:4]

#define

plugin drlc opt out [endpoint:1] [eventId:4]

#define

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_CLEAR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_CLEAR

plugin drlc clear [endpoint:1]

  • Clear the load control event table.

    • endpoint - INT8U - The relevant endpoint.


Definition at line 2533 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_IN#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_IN

plugin drlc opt in [endpoint:1] [eventId:4]

  • Modify the entry in the clients load control event table to opt in for a scheduled load control event.

    • endpoint - INT8U - The relevant endpoint.

    • eventId - INT32U - The event id of the event that the user is opting in or out of.


Definition at line 2540 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_OUT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_OPT_OUT

plugin drlc opt out [endpoint:1] [eventId:4]

  • Modify the entry in the clients load control event table to opt out of a scheduled load control event.

    • endpoint - INT8U - The relevant endpoint.

    • eventId - INT32U - The event id of the event that the user is opting in or out of.


Definition at line 2547 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DRLC_PLUGIN_DRLC_PRINT

plugin drlc print [endpoint:1]

  • Print the Demand Response Load Control Table.

    • endpoint - INT8U - The relevant endpoint.


Definition at line 2553 of file ./app/framework/test/headers/cli.doc