ZigBee Device Object Commands (ZDO)#

Commands related to the management of a ZigBee device including device discovery and commissioning.

Macros#

#define
#define

zdo bind [destination:2] [source Endpoint:1] [destEndpoint:1] [cluster:2] [remoteEUI64:8] [destEUI64:8]

#define
#define

zdo in-cl-list add [clusterId:2]

#define

zdo leave [target:2] [removeChildren:1] [rejoin:1]

#define

zdo match [nodeId:2] [profile:2]

#define

zdo mgmt-bind [target:2] [startIndex:1]

#define

zdo mgmt-lqi [target:2] [startIndex:1]

#define
#define
#define

zdo nwk-upd chanPg [channel:1] [page:1]

#define

zdo nwk-upd scan [targetNodeId:2] [scanDuration:1] [scanCount:2]

#define

zdo nwk-upd scan-chan-mask [targetNodeId:2] [scanDuration:1] [scanCount:2] [channelMask:4]

#define

zdo nwk-upd set [nwkMgrId:2] [channelMask:4]

#define

zdo out-cl-list add [clusterId:2]

#define
#define

zdo route [target:2] [index:1]

#define

zdo simple [dest:2] [targetEndpoint:1]

#define

zdo unbind group [target:2] [source eui64:8] [source endpoint:1] [clusterID:2] [groupAddress:2]

#define

zdo unbind unicast [target:2] [source eui64:8] [source endpoint:1] [clusterID:2] [destinationEUI64:8] [destEndpoint:1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_ACTIVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_ACTIVE

zdo active [nodeId:2]

  • Send an active endpoint request to the device with the given short id.

    • nodeId - INT16U - Two byte short id, destination for the active endpoint request


Definition at line 707 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_BIND#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_BIND

zdo bind [destination:2] [source Endpoint:1] [destEndpoint:1] [cluster:2] [remoteEUI64:8] [destEUI64:8]

  • Send a ZDO Bind command to a device specified in the command arguments.

    • destination - INT16U - Two byte destination node id

    • source Endpoint - INT8U - Remote device's source endpoint to bind

    • destEndpoint - INT8U - Remote endpoint to bind

    • cluster - INT16U - Cluster on which to bind

    • remoteEUI64 - IEEE_ADDRESS - Remote node EUI64

    • destEUI64 - IEEE_ADDRESS - Binding's dest EUI64. Usually the local node's EUI64


Definition at line 718 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_IEEE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_IEEE

zdo ieee [nodeId:2]

  • Request an ieee address based on a given node id.

    • nodeId - INT16U - Short address of the device for which a long address is requested


Definition at line 724 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_IN_CL_LIST_ADD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_IN_CL_LIST_ADD

zdo in-cl-list add [clusterId:2]

  • Add clusters to the known server (in) clusters on this device.

    • clusterId - INT16U - Server cluster id


Definition at line 730 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_IN_CL_LIST_CLEAR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_IN_CL_LIST_CLEAR

zdo in-cl-list clear

  • Clear the ZDO list of server (in) clusters.


Definition at line 735 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_LEAVE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_LEAVE

zdo leave [target:2] [removeChildren:1] [rejoin:1]

  • Send a ZDO Management Leave command to the target device.

    • target - INT16U - Target node ID

    • removeChildren - BOOLEAN - Remove children

    • rejoin - BOOLEAN - Rejoin after leave


Definition at line 743 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_MATCH#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_MATCH

zdo match [nodeId:2] [profile:2]

  • Sends a matchDescriptorsRequest to the given destination with the given profile.

    • nodeId - INT16U - Two byte node id indicating wher

    • profile - INT16U - Two byte profile id for the match descriptor request


Definition at line 750 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_MGMT_BIND#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_MGMT_BIND

zdo mgmt-bind [target:2] [startIndex:1]

  • Send a ZDO MGMT-Bind (Binding Table) Request to the target device.

    • target - INT16U - Target node ID

    • startIndex - INT8U - Starting index into table query


Definition at line 757 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_MGMT_LQI#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_MGMT_LQI

zdo mgmt-lqi [target:2] [startIndex:1]

  • Send a ZDO MGMT-LQI (LQI Table) Request to the target device.

    • target - INT16U - Target node ID

    • startIndex - INT8U - Starting index into table query


Definition at line 764 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NODE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NODE

zdo node [target:2]

  • Sends a node descriptor request to a given target device

    • target - INT16U - Two byte address for the target device.


Definition at line 770 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK

zdo nwk [ieee:8]

  • Sends a network address request for the given IEEE address.

    • ieee - IEEE_ADDRESS - IEEE address for which a short address is being requested


Definition at line 776 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_CHAN#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_CHAN

zdo nwk-upd chan [channel:1]

  • Sends an update channel request.

    • channel - INT8U - One byte channel to change to.


Definition at line 782 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_CHAN_PG#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_CHAN_PG

zdo nwk-upd chanPg [channel:1] [page:1]

  • Sends an update channel page request. The stack shall send network enhanced update request if page is non-zero.

    • channel - INT8U - One byte channel to change to.

    • page - INT8U - One byte page to change to.


Definition at line 789 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_SCAN#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_SCAN

zdo nwk-upd scan [targetNodeId:2] [scanDuration:1] [scanCount:2]

  • Performs an energy scan.

    • targetNodeId - INT16U - Two byte short id of the target device

    • scanDuration - INT8U - One byte scan duration. Must be in range 0 - 5

    • scanCount - INT16U - Number of scans to perform. Must be in range 1 - 8


Definition at line 797 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_SCAN_CHAN_MASK#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_SCAN_CHAN_MASK

zdo nwk-upd scan-chan-mask [targetNodeId:2] [scanDuration:1] [scanCount:2] [channelMask:4]

  • Performs an energy scan on given channel mask. This can be used to perform scanning with page number embedded in channel mask, it mainly used for subghz network. The stack shall send network enhanced update request if page is non-zero.

    • targetNodeId - INT16U - Two byte short id of the target device

    • scanDuration - INT8U - One byte scan duration. Must be in range 0 - 5

    • scanCount - INT16U - Number of scans to perform. Must be in range 1 - 8

    • channelMask - INT32U - Four byte channel mask


Definition at line 806 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_SET#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_NWK_UPD_SET

zdo nwk-upd set [nwkMgrId:2] [channelMask:4]

  • Broadcasts the ID of the new network manager and active channels.

    • nwkMgrId - INT16U - Two byte network manager id

    • channelMask - INT32U - Four byte channel mask


Definition at line 813 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_OUT_CL_LIST_ADD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_OUT_CL_LIST_ADD

zdo out-cl-list add [clusterId:2]

  • Add clusters to the known client (out) clusters on this device.

    • clusterId - INT16U - Client cluster ids


Definition at line 819 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_OUT_CL_LIST_CLEAR#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_OUT_CL_LIST_CLEAR

zdo out-cl-list clear

  • Clear the ZDO list of client (out) clusters.


Definition at line 824 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_POWER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_POWER

zdo power [target:2]

  • Send a ZDO Power Descriptor Request to the target device.

    • target - INT16U - Target node ID


Definition at line 830 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_ROUTE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_ROUTE

zdo route [target:2] [index:1]

  • Send a ZDO route request command to the target.

    • target - INT16U - Target node ID

    • index - INT8U - The index of the remote node's routing table to request.


Definition at line 837 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_SIMPLE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_SIMPLE

zdo simple [dest:2] [targetEndpoint:1]

  • Sends out a simple descriptor request for the short address and endpoint specified.

    • dest - INT16U - Short address of the device where the simple descriptor request should be sent

    • targetEndpoint - INT8U - The endpoint on the target device where the simple descriptor request will be sent


Definition at line 844 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_UNBIND_GROUP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_UNBIND_GROUP

zdo unbind group [target:2] [source eui64:8] [source endpoint:1] [clusterID:2] [groupAddress:2]

  • Sends an unbind request for a multicast binding to the target device.

    • target - INT16U - Target node ID

    • source eui64 - IEEE_ADDRESS - The source EUI64 of the binding (the remote device's EUI64)

    • source endpoint - INT8U - The source endpoint of the binding.

    • clusterID - INT16U - The cluster ID to unbind.

    • groupAddress - INT16U - The group address in the binding


Definition at line 854 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_UNBIND_UNICAST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_ZDO_ZDO_UNBIND_UNICAST

zdo unbind unicast [target:2] [source eui64:8] [source endpoint:1] [clusterID:2] [destinationEUI64:8] [destEndpoint:1]

  • Sends an unbind request for a unicast binding to the target device.

    • target - INT16U - Target node ID

    • source eui64 - IEEE_ADDRESS - The source EUI64 of the binding (the remote device's EUI64)

    • source endpoint - INT8U - The source endpoint of the binding.

    • clusterID - INT16U - The cluster ID to unbind.

    • destinationEUI64 - IEEE_ADDRESS - The destination EUI64 in the binding (usually the local node's EUI64

    • destEndpoint - INT8U - The destination endpoint of the binding


Definition at line 865 of file ./app/framework/test/headers/cli.doc