Plugin Commands: GBCS Device Log#
The gbcs-device-log plugin contributes several CLI commands to the application framework to be used in configuring and managing the GBCS Device Log.
Macros#
plugin gbcs-device-log clear
plugin gbcs-device-log count
plugin gbcs-device-log exists [deviceId:8] [deviceType:1]
plugin gbcs-device-log fill
plugin gbcs-device-log get [deviceId:8]
plugin gbcs-device-log is-sleepy [deviceType:1]
plugin gbcs-device-log print
plugin gbcs-device-log remove [deviceId:8]
plugin gbcs-device-log reset
plugin gbcs-device-log store [deviceId:8] [deviceType:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_CLEAR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_CLEAR
plugin gbcs-device-log clear
Clear all entries from the GBCS Device Log.
3194
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_COUNT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_COUNT
plugin gbcs-device-log count
Get the number of entries in the GBCS Device Log.
3199
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_EXISTS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_EXISTS
plugin gbcs-device-log exists [deviceId:8] [deviceType:1]
Check to see if a device exists in the GBCS Device Log.
deviceId - IEEE_ADDRESS - The EUI64 of the device in question
deviceType - INT8U - The GBCS device type of the device in question
3206
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_FILL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_FILL
plugin gbcs-device-log fill
Helper command to fill the GBCS Device Log with random info.
3211
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_GET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_GET
plugin gbcs-device-log get [deviceId:8]
Get device info about an entry in the GBCS Device Log
deviceId - IEEE_ADDRESS - The EUI64 of the device for which information is requested
3217
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_IS_SLEEPY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_IS_SLEEPY
plugin gbcs-device-log is-sleepy [deviceType:1]
Is the given device type a sleepy device.
deviceType - INT8U - The GBCS device type to be checked
3223
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_PRINT
plugin gbcs-device-log print
Print all entries in the GBCS Device log.
3228
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_REMOVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_REMOVE
plugin gbcs-device-log remove [deviceId:8]
Remove an entry from the GBCS Device Log.
deviceId - IEEE_ADDRESS - The EUI64 of the device to be removed
3234
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_RESET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_RESET
plugin gbcs-device-log reset
Reset the GBCS Device Log to include just those entries configured with the plugin.
3239
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_STORE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GBCS_DEVICE_LOG_PLUGIN_GBCS_DEVICE_LOG_STORE
plugin gbcs-device-log store [deviceId:8] [deviceType:1]
Add or update an entry within the GBCS Device Log.
deviceId - IEEE_ADDRESS - The EUI64 of the device to be added or updated
deviceType - INT8U - The GBCS device type of the device to be added or updated
3246
of file ./app/framework/test/headers/cli.doc