Plugin Commands: BLE#

The BLE plugin contributes CLI commands to the application framework to be used for initiating actions at the BLE stack.

Macros#

#define

plugin ble connection close [connection-handle:1]

#define

plugin ble gap conn-open [address:-1] [address-type:1]

#define

plugin ble gap discover [discovery-mode:1]

#define

plugin ble gap set-adv-params [min-interval:2] [max-interval:2] [channel-map:1]

#define

plugin ble gap set-bt5-mode [advertisement-handle:1] [discoverable-mode:1] [connectable-mode:1] [max-events:2] [address-type:1]

#define

plugin ble gap set-conn-params [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2]

#define

plugin ble gap set-mode [discoverable-mode:1] [connectable-mode:1]

#define

plugin ble gap update-conn-params [connection-handle:2] [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2]

#define

plugin ble gatt discover-characteristics [connection-handle:1] [serice-handle:4]

#define

plugin ble gatt discover-primary-services [connection-handle:1]

#define

plugin ble gatt set-characteristic-notification [connection-handle:1] [characteristic-handle:2] [flags:1]

#define

plugin ble gatt write-characteristic [connection-handle:1] [characteristic-handle:2] [value-len:1] [value-data:-1]

#define

plugin ble sm configure [flags:1] [io_capability:1]

#define

plugin ble sm confirm-passkey [connection:1] [confirm:1]

#define

plugin ble sm delete-bonding [bonding-handle:1]

#define

plugin ble sm enter-passkey [connection:1] [passkey:4]

#define

plugin ble sm increase-security [connection-handle:1]

#define

plugin ble sm set-bondable-mode [bondable-mode:1]

#define

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_CONNECTION_CLOSE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_CONNECTION_CLOSE

plugin ble connection close [connection-handle:1]

  • Close BLE connection

    • connection-handle - INT8U - the connection handle which should be closed


Definition at line 1460 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_CONN_OPEN#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_CONN_OPEN

plugin ble gap conn-open [address:-1] [address-type:1]

  • Open a GAP connection

    • address - OCTET_STRING - The BLE address of the target device

    • address-type - INT8U - The address type: 0=public, 1=random, 2=public resolved by the stack, 3=public resolved by the stack, 16=classic bluetooth


Definition at line 1467 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_DISCOVER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_DISCOVER

plugin ble gap discover [discovery-mode:1]

  • Start a GAP discovery procedure

    • discovery-mode - INT8U - The GAP discovery mode: 0=only limited discoverable devices, 1=limited and generic discoverable devices, 2=all devices


Definition at line 1473 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_ADV_PARAMS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_ADV_PARAMS

plugin ble gap set-adv-params [min-interval:2] [max-interval:2] [channel-map:1]

  • Set the GAP advertisement parameters

    • min-interval - INT16U - minimum connection interval

    • max-interval - INT16U - maximum connection interval

    • channel-map - INT8U - Channel map indicating which of three channels will be used


Definition at line 1481 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_BT5_MODE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_BT5_MODE

plugin ble gap set-bt5-mode [advertisement-handle:1] [discoverable-mode:1] [connectable-mode:1] [max-events:2] [address-type:1]

  • Set the BT5 GAP mode

    • advertisement-handle - INT8U - The handle index of advertisement

    • discoverable-mode - INT8U - The GAP discoverable mode: 0=non discoverable, 1=limited discoverable, 2=general discoverable, 3=broadcast, 4=user data

    • connectable-mode - INT8U - The GAP connectable mode: 0=non connectable, 1=directed connectable, 2=undirected connectable, 3=scannable non connectable

    • max-events - INT16U - The maximum number of events

    • address-type - INT8U - Address type: 0=public, 1=random, 2=public identity, 3=random identity, 16=classic bluetooth


Definition at line 1491 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_CONN_PARAMS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_CONN_PARAMS

plugin ble gap set-conn-params [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2]

  • Set the GAP connection parameters

    • min-interval - INT16U - minimum connection event interval

    • max-interval - INT16U - maximum connection event interval

    • slave-latency - INT16U - number of connection intervals the slave can skip

    • supervision-timeout - INT16U - time before the connection is dropped


Definition at line 1500 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_MODE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_SET_MODE

plugin ble gap set-mode [discoverable-mode:1] [connectable-mode:1]

  • Set the GAP mode

    • discoverable-mode - INT8U - The GAP discoverable mode: 0=non discoverable, 1=limited discoverable, 2=general discoverable, 3=broadcast, 4=user data

    • connectable-mode - INT8U - The GAP connectable mode: 0=non connectable, 1=directed connectable, 2=undirected connectable, 3=scannable non connectable


Definition at line 1507 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_UPDATE_CONN_PARAMS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GAP_UPDATE_CONN_PARAMS

plugin ble gap update-conn-params [connection-handle:2] [min-interval:2] [max-interval:2] [slave-latency:2] [supervision-timeout:2]

  • Set the GAP connection parameters for connection

    • connection-handle - INT16U - connection handle

    • min-interval - INT16U - minimum connection event interval

    • max-interval - INT16U - maximum connection event interval

    • slave-latency - INT16U - number of connection intervals the slave can skip

    • supervision-timeout - INT16U - time before the connection is dropped


Definition at line 1517 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_CHARACTERISTICS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_CHARACTERISTICS

plugin ble gatt discover-characteristics [connection-handle:1] [serice-handle:4]

  • GATT discovery of characteristics

    • connection-handle - INT8U - the connection handle on which discovery should be performed

    • serice-handle - INT32U - the service handle on which discovery should be performed


Definition at line 1524 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_PRIMARY_SERVICES#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_DISCOVER_PRIMARY_SERVICES

plugin ble gatt discover-primary-services [connection-handle:1]

  • GATT discovery of primary services

    • connection-handle - INT8U - the connection handle on which discovery should be performed


Definition at line 1530 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_SET_CHARACTERISTIC_NOTIFICATION#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_SET_CHARACTERISTIC_NOTIFICATION

plugin ble gatt set-characteristic-notification [connection-handle:1] [characteristic-handle:2] [flags:1]

  • GATT set characteristic notification

    • connection-handle - INT8U - the connection handle for which the notification should be set

    • characteristic-handle - INT16U - the characteristic handle to set notification for

    • flags - INT8U - 0=disable, 1=notification, 2=indication


Definition at line 1538 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_WRITE_CHARACTERISTIC#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GATT_WRITE_CHARACTERISTIC

plugin ble gatt write-characteristic [connection-handle:1] [characteristic-handle:2] [value-len:1] [value-data:-1]

  • GATT write characteristic value

    • connection-handle - INT8U - the connection handle

    • characteristic-handle - INT16U - the characteristic handle

    • value-len - INT8U - the lenght of data

    • value-data - OCTET_STRING - data to write


Definition at line 1547 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GET_ADDRESS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_GET_ADDRESS

plugin ble get address

  • Read the Bluetooth address


Definition at line 1552 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_HELLO#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_HELLO

plugin ble hello

  • Can be used to check that Bluetooth stack is functional


Definition at line 1557 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_CONFIGURE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_CONFIGURE

plugin ble sm configure [flags:1] [io_capability:1]

  • Configure security requirements and I/O capabilities of the system; See https://docs.silabs.com/bluetooth/latest/sm for more information

    • flags - INT8U - Security requirement bitmask.

    • io_capability - INT8U - I/O Capabilities


Definition at line 1564 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_CONFIRM_PASSKEY#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_CONFIRM_PASSKEY

plugin ble sm confirm-passkey [connection:1] [confirm:1]


Definition at line 1571 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_ALL_BONDINGS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_ALL_BONDINGS

plugin ble sm delete-all-bondings


Definition at line 1576 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_BONDING#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_DELETE_BONDING

plugin ble sm delete-bonding [bonding-handle:1]


Definition at line 1582 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_ENTER_PASSKEY#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_ENTER_PASSKEY

plugin ble sm enter-passkey [connection:1] [passkey:4]


Definition at line 1589 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_INCREASE_SECURITY#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_INCREASE_SECURITY

plugin ble sm increase-security [connection-handle:1]


Definition at line 1595 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_LIST_ALL_BONDINGS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_LIST_ALL_BONDINGS

plugin ble sm list-all-bondings


Definition at line 1600 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_SET_BONDABLE_MODE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SM_SET_BONDABLE_MODE

plugin ble sm set-bondable-mode [bondable-mode:1]


Definition at line 1606 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SYSTEM_SET_TX_POWER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_BLE_PLUGIN_BLE_SYSTEM_SET_TX_POWER

plugin ble system set-tx-power [tx-power:2]

  • Set the TX power

    • tx-power - INT16S - tx power to be set in 0.1dBm steps


Definition at line 1612 of file ./app/framework/test/headers/cli.doc