Plugin Commands: Tunneling Client#

The Tunneling Client Plugin contributes several commands to the application framework's CLI. These commands may be used to create messages related to opening and closing a tunnel between two devices.

Macros#

#define

plugin tunneling-client request [server:2] [clientEndpoint:1] [serverEndpoint:1] [protocolId:1] [manufacturerCode:2] [flowControlSupport:1]

#define

plugin tunneling-client transfer [tunnelIndex:1] [data:-1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_CLOSE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_CLOSE

plugin tunneling-client close [tunnelIndex:1]

  • Close a Tunneling cluster tunnel.

    • tunnelIndex - INT8U - The index of the tunnel to close.


Definition at line 7089 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_PRINT

plugin tunneling-client print

  • Print out the status of active tunnels.


Definition at line 7094 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_REQUEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_REQUEST

plugin tunneling-client request [server:2] [clientEndpoint:1] [serverEndpoint:1] [protocolId:1] [manufacturerCode:2] [flowControlSupport:1]

  • Request a Tunneling cluster tunnel with a server.

    • server - INT16U - The network address of the server to which the request will be sent.

    • clientEndpoint - INT8U - The local endpoint from which the request will be sent.

    • serverEndpoint - INT8U - The remote endpoint to which the request will be sent.

    • protocolId - INT8U - The protocol id of the requested tunnel.

    • manufacturerCode - INT16U - The manufacturer code of the requested tunnel.

    • flowControlSupport - BOOLEAN - 1 if flow control support is requested or 0 if not.


Definition at line 7105 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_TRANSFER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TUNNELING_CLIENT_PLUGIN_TUNNELING_CLIENT_TRANSFER

plugin tunneling-client transfer [tunnelIndex:1] [data:-1]

  • Transfer data to a server through a Tunneling cluster tunnel.

    • tunnelIndex - INT8U - The index of the tunnel through which to send the data.

    • data - OCTET_STRING - The data to send through the tunnel.


Definition at line 7112 of file ./app/framework/test/headers/cli.doc