Test Harness#

All commands related to the testing of a device.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_TEST_ZCL_TEST_RESPONSE_OFF#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_TEST_ZCL_TEST_RESPONSE_OFF

zcl test response off

  • Sets a flag so that the application framework WILL NOT respond to the next ZCL message that comes in over the air.


Definition at line 686 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_TEST_ZCL_TEST_RESPONSE_ON#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_TEST_ZCL_TEST_RESPONSE_ON

zcl test response on

  • Sets a flag so that the application framework WILL respond to the next ZCL message that comes in over the air.


Definition at line 691 of file ./app/framework/test/headers/cli.doc