Plugin Commands: Manufacturing Library CLI#

CLI commands related to the manufacturing library.

Macros#

#define
#define
#define
#define

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_MFGENABLE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_MFGENABLE

plugin mfglib mfgenable [enabled:1]

  • Enable mfglib.

    • enabled - INT8U - 1 = enable, 0 = disable.


Definition at line 3961 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_PROGRAM_EUI#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_PROGRAM_EUI

plugin mfglib programEui [duration:8]

  • Program EUI.

    • duration - IEEE_ADDRESS - IEEE address to program.


Definition at line 3967 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_MESSAGE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_MESSAGE

plugin mfglib send message [data:-1] [numPackets:2]

  • Send a test message with the specified data in it.

    • data - OCTET_STRING - The hex data to send, up to 16 bytes.

    • numPackets - INT16U - The number of packets to send.


Definition at line 3974 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_RANDOM#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_RANDOM

plugin mfglib send random [numPackets:2] [length:1]

  • Send a series of test packets with random data..

    • numPackets - INT16U - The number of packets to send.

    • length - INT8U - The length of the packet to send.


Definition at line 3981 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_TEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SEND_TEST

plugin mfglib send test [numPackets:2] [length:1]

  • Send a series of test packets with fixed data.

    • numPackets - INT16U - The number of packets to send.

    • length - INT8U - The length of the packet to send.


Definition at line 3988 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_CHANNEL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_CHANNEL

plugin mfglib set-channel [channel:1]

  • Sets the channel used by the manufacturing library for testing.

    • channel - INT8U - The 802.15.4 channel number.


Definition at line 3994 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_OPTIONS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_OPTIONS

plugin mfglib set-options [options:1]

  • Sets options in the manufacturing library for testing.

    • options - INT8U - The options bitmask (0 = normal transmit, 1 = CSMA transmit).


Definition at line 4000 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_POWER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SET_POWER

plugin mfglib set-power [powerLevel:1] [powerMode:2]

  • Set the power level and mode for the manufacturing test.

    • powerLevel - INT8S - The power level

    • powerMode - INT16U - The power mode


Definition at line 4007 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SLEEP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_SLEEP

plugin mfglib sleep [duration:2]

  • Sleep.

    • duration - INT16U - Sleep duration (mS).


Definition at line 4013 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_START#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_START

plugin mfglib start [useCallback:1]

  • Start the mfglib test mode.

    • useCallback - BOOLEAN - Use the Rx callback.


Definition at line 4019 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STATUS#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STATUS

plugin mfglib status

  • Prints the current status of the manufacturing library.


Definition at line 4024 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STOP

plugin mfglib stop

  • Stop the mfglib test mode.


Definition at line 4029 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STREAM_START#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STREAM_START

plugin mfglib stream start

  • Start the stream test.


Definition at line 4034 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STREAM_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_STREAM_STOP

plugin mfglib stream stop

  • Stop the stream test.


Definition at line 4039 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_TONE_START#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_TONE_START

plugin mfglib tone start

  • Starts a tone test.


Definition at line 4044 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_TONE_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MANUFACTURING_LIBRARY_CLI_PLUGIN_MFGLIB_TONE_STOP

plugin mfglib tone stop

  • Stops the tone test.


Definition at line 4049 of file ./app/framework/test/headers/cli.doc