Cluster Commands: Basic#
This group describes the CLI commands for the Basic cluster. Listed below is a description of the cluster: Attributes for determining basic information about a device, setting user device information such as location, and enabling a device.
Macros#
zcl basic rtfd
zcl basic gls [startLocale:-1] [maxLocalesRequested:1]
zcl basic glsr [discoveryComplete:1] [localeSupported:-1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_RTFD#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_RTFD
zcl basic rtfd
Command that resets all attribute values to factory default.
8220
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLS
zcl basic gls [startLocale:-1] [maxLocalesRequested:1]
This command gets locales supported.
startLocale - CHAR_STRING
maxLocalesRequested - INT8U
8227
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLSR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_BASIC_GLSR
zcl basic glsr [discoveryComplete:1] [localeSupported:-1]
The locales supported response command is sent in response to a get locales supported command, and is used to discover which locales the device supports.
discoveryComplete - INT8U
localeSupported - CHAR_STRING
8234
of file ./app/framework/test/headers/cli.doc