Plugin Commands: Sub-GHz Client#
The Sub-GHz commands provide commands for sub-GHz duty cycle, power management and frequency agility.
Macros#
plugin sub-ghz get-suspend-status [nodeId:2] [ep:1]
plugin sub-ghz ignore-suspend-status [ignore:1]
plugin sub-ghz request-channel-change [nodeId:2] [page:1] [channel:1] [macTxUcastTotal:2] [macTxUcastFailures:2] [macTxUcastRetries:2] [period:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_GET_SUSPEND_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_GET_SUSPEND_STATUS
plugin sub-ghz get-suspend-status [nodeId:2] [ep:1]
Send the GetSuspendZCLMessagesStatus command to the Sub-GHz server.
nodeId - INT16U - Server's node ID
ep - INT8U - Server's endpoint
6447
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_IGNORE_SUSPEND_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_IGNORE_SUSPEND_STATUS
plugin sub-ghz ignore-suspend-status [ignore:1]
Ignore the suspend status when sending ZCL messages (for testing purposes only).
ignore - BOOLEAN - Whether or not the suspend status should be ignored
6453
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_REQUEST_CHANNEL_CHANGE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_CLIENT_PLUGIN_SUB_GHZ_REQUEST_CHANNEL_CHANGE
plugin sub-ghz request-channel-change [nodeId:2] [page:1] [channel:1] [macTxUcastTotal:2] [macTxUcastFailures:2] [macTxUcastRetries:2] [period:1]
Send the Mgmt_NWK_Unsolicited_Enhanced_Update_notify command to the Sub-GHz server.
nodeId - INT16U - Server's node ID
page - INT8U - Current channel page
channel - INT8U - Current channel
macTxUcastTotal - INT16U - Total number of Mac Tx transaction attempts
macTxUcastFailures - INT16U - Total number of Mac Tx transaction failures
macTxUcastRetries - INT16U - Total number of Mac Tx transaction retries
period - INT8U - Time in minutes over which the Mac Tx counts were measured
6465
of file ./app/framework/test/headers/cli.doc