Plugin Commands: Sub-GHz Server#
The Sub-GHz commands provide commands for sub-GHz duty cycle, power management and frequency agility.
Macros#
plugin sub-ghz channel-change print
plugin sub-ghz channel-change set [value:4]
plugin sub-ghz channel-mask print
plugin sub-ghz channel-mask set [mask1:4] [mask2:4] [mask3:4] [mask4:4]
plugin sub-ghz client-status [nodeId:2]
plugin sub-ghz limits print
plugin sub-ghz limits set [limited:2] [critical:2] [suspended:2]
plugin sub-ghz suspend-zcl-messages [nodeId:2] [ep:1] [period:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_CHANGE_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_CHANGE_PRINT
plugin sub-ghz channel-change print
Print out the status of the sub-GHz channel change attribute.
6480
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_CHANGE_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_CHANGE_SET
plugin sub-ghz channel-change set [value:4]
Set the status of the sub-GHz channel change attribute.
value - INT32U - Channel change attribute (bit mask)
6486
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_MASK_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_MASK_PRINT
plugin sub-ghz channel-mask print
Print out the status of all sub-GHz channel masks.
6491
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_MASK_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CHANNEL_MASK_SET
plugin sub-ghz channel-mask set [mask1:4] [mask2:4] [mask3:4] [mask4:4]
Set one or more sub-GHz channel mask(s).
mask1 - INT32U - Channel 28 mask
mask2 - INT32U - Channel 29 mask
mask3 - INT32U - Channel 30 mask
mask4 - INT32U - Channel 31 mask
6500
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CLIENT_STATUS#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_CLIENT_STATUS
plugin sub-ghz client-status [nodeId:2]
Print the given Sub-GHZ given client's current status.
nodeId - INT16U - Client's Node ID of the given client
6506
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_LIMITS_PRINT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_LIMITS_PRINT
plugin sub-ghz limits print
Print the current Duty Cycle limits.
6511
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_LIMITS_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_LIMITS_SET
plugin sub-ghz limits set [limited:2] [critical:2] [suspended:2]
Set the Duty Cycle limits.
limited - INT16U - 'Limited' Duty Cycle state threshold in % * 100 (i.e. 150 = 1.5%)
critical - INT16U - 'Critical' Duty Cycle state threshold in % * 100
suspended - INT16U - 'Suspended' Duty Cycle state threshold in % * 100
6519
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_SUSPEND_ZCL_MESSAGES#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SUB_GHZ_SERVER_PLUGIN_SUB_GHZ_SUSPEND_ZCL_MESSAGES
plugin sub-ghz suspend-zcl-messages [nodeId:2] [ep:1] [period:1]
Send the SuspendZCLMessages command to the given client.
nodeId - INT16U - Node ID of the given client
ep - INT8U - Endpoint of the given client
period - INT8U - Period in minutes
6527
of file ./app/framework/test/headers/cli.doc