Network#
The Network command set provides commands for interacting with the network. This includes building as well as sending ZigBee commands out on to the network.
Macros#
network broad-pjoin [seconds:1]
network change-channel [channel:1]
network change-keep-alive-mode [keepAliveMode:1]
network extpanid [extPanId:-1]
network find joinable
network find unused
network form [channel:1] [power:1] [panId:2]
network init
network isopen
network join [channel:1] [power:1] [panId:2]
network leave
network multi-phy-start [page:1] [channel:1] [power:1]
network multi-phy-stop
network pjoin [seconds:1]
network rejoin [haveCurrentNetworkKey:1] [channelMask:4]
network rejoin-diff-device-type [haveCurrentNetworkKey:1] [channelMask:4] [nodeType:1]
network set [networkIndex:1]
network timeout-option-mask [mask:2]
option apsretry default
option apsretry off
option apsretry on
option binding-table clear
option binding-table set [bindingTableIndex:1] [clusterId:2] [localEndpoint:1] [remoteEndpoint:1] [ieeeAddress:8]
option disc [profileId:2] [clusterId:2]
option edb [endpoint:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_BROAD_PJOIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_BROAD_PJOIN
network broad-pjoin [seconds:1]
Permit joining on the network for a given number of seconds AND broadcast a ZDO Mgmt Permit Joining request to all routers.
seconds - INT8U - Number of seconds during which devices will be allowed to join the network. A value of 0xff turns permit joining on permanently
413
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_CHANGE_CHANNEL#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_CHANGE_CHANNEL
network change-channel [channel:1]
Attempts to change device over to a different channel given in the channel argument.
channel - INT8U - The channel to change to.
419
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_CHANGE_KEEP_ALIVE_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_CHANGE_KEEP_ALIVE_MODE
network change-keep-alive-mode [keepAliveMode:1]
Switch between different keep alive modes supported by a router
keepAliveMode - INT8U - The keep alive mode.
425
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_EXTPANID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_EXTPANID
network extpanid [extPanId:-1]
Write the extended pan id for the device.
extPanId - OCTET_STRING - The bytes for the extended pan id
431
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_JOINABLE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_JOINABLE
network find joinable
Begin a search for a joinable network. Will automatically attempt to join the first network that it finds.
436
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_UNUSED#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FIND_UNUSED
network find unused
Begin a search for an unused Channel and Pan Id. Will automatically form a network on the first unused Channel and Pan Id it finds.
441
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FORM#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_FORM
network form [channel:1] [power:1] [panId:2]
Create a network on the given channel, power and panId.
channel - INT8U - The channel on which to form the network
power - INT8S - One byte signed value indicating the TX power that the radio should be set to
panId - INT16U - Two byte pan id for the network
449
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_ID#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_ID
network id
Prints the current Node ID, EUI64, and Pan ID.
454
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_INIT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_INIT
network init
Initialize a network; this is a test command used for tc-swap-out testing.
459
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_ISOPEN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_ISOPEN
network isopen
Check if and for how long the network is open.
464
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_JOIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_JOIN
network join [channel:1] [power:1] [panId:2]
Join an existing network on the given channel, power and panId.
channel - INT8U - The channel on which to form the network
power - INT8S - One byte signed value indicating the TX power that the radio should be set to
panId - INT16U - Two byte pan id for the network
472
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_LEAVE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_LEAVE
network leave
Leave the current network.
477
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_START
network multi-phy-start [page:1] [channel:1] [power:1]
To start multi phy interface other than native and form the network. The stack uses same PanId as native radio network.
page - INT8U - The page on which to form the network.
channel - INT8U - The channel on which to form the network.
power - INT8S - One byte signed value indicating the TX power that the radio should be set to
485
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_STOP#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_MULTI_PHY_STOP
network multi-phy-stop
Terminates the multi phy interface
490
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_PJOIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_PJOIN
network pjoin [seconds:1]
Permit joining on the network for a given number of seconds
seconds - INT8U - Number of seconds during which devices will be allowed to join the network. A value of 0xff turns permit joining on permanently
496
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN
network rejoin [haveCurrentNetworkKey:1] [channelMask:4]
Rejoin an existing network in a secure or insecure manner.
haveCurrentNetworkKey - INT8U - Boolean indicating whether the device can rejoin secure or not. 1=rejoin with encryption, 0=rejoin without encryption
channelMask - INT32U - 4 byte channel mask which should be used to search for the network to rejoin.
503
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN_DIFF_DEVICE_TYPE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_REJOIN_DIFF_DEVICE_TYPE
network rejoin-diff-device-type [haveCurrentNetworkKey:1] [channelMask:4] [nodeType:1]
Rejoin an existing network in a secure or insecure manner with a different device type.
haveCurrentNetworkKey - INT8U - Boolean indicating whether the device can rejoin secure or not. 1=rejoin with encryption, 0=rejoin without encryption
channelMask - INT32U - 4 byte channel mask which should be used to search for the network to rejoin.
nodeType - INT8U - An enumeration indicating the device type to rejoin as.The stack only accepts EMBER_END_DEVICE and EMBER_SLEEPY_END_DEVICE.
511
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_SET
network set [networkIndex:1]
Set the network index used by all future CLI commands. Before executing a CLI command, the framework will switch to this network. After the command finishes executing, the framework will switch back to the previous network. The CLI uses the same network index until the device resets or it is changed through this command.
networkIndex - INT8U - The network index to use for CLI commands
517
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_TIMEOUT_OPTION_MASK#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_NETWORK_TIMEOUT_OPTION_MASK
network timeout-option-mask [mask:2]
Attempts to change child timeout option mask to filter out undesirable values (e.g. no more than 3 days).
mask - INT16U - The timeout option mask.
523
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_DEFAULT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_DEFAULT
option apsretry default
Forces the AppFramework to set/clear the APS Retry option (in APS Frame options mask) for all subsequent outgoing messages; a value of "default" allows the AppFramework to use its own default logic to determine when the APS Retry option should be used.
528
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_OFF#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_OFF
option apsretry off
Forces the AppFramework to set/clear the APS Retry option (in APS Frame options mask) for all subsequent outgoing messages; Turns APS retry off
533
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_ON#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_APSRETRY_ON
option apsretry on
Forces the AppFramework to set/clear the APS Retry option (in APS Frame options mask) for all subsequent outgoing messages; Turns APS retry on.
538
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_CLEAR#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_CLEAR
option binding-table clear
Clear the binding table
543
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_SET#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_BINDING_TABLE_SET
option binding-table set [bindingTableIndex:1] [clusterId:2] [localEndpoint:1] [remoteEndpoint:1] [ieeeAddress:8]
Set a binding table entry for the arguments specified.
bindingTableIndex - INT8U - one byte index into the binding table
clusterId - INT16U - cluster id to send with the discovery message
localEndpoint - INT8U - local endpoint to bind
remoteEndpoint - INT8U - remote endpoint to bind
ieeeAddress - IEEE_ADDRESS - 8 byte IEEE address provided big endian
553
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_DISC#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_DISC
option disc [profileId:2] [clusterId:2]
Sends a ZDO Match Descriptor Request for the server side of the specified cluster from the specified application profile. Match Descriptor Responses received are printed to the serial output.
profileId - INT16U - the profile id to send with the discovery message
clusterId - INT16U - cluster id to send with the discovery message
560
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_EDB#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_NETWORK_OPTION_EDB
option edb [endpoint:1]
Sends a ZDO End Device Bind Request using the given local endpoint.
endpoint - INT8U - The local endpoint whose simple descriptor will be used to create the request
566
of file ./app/framework/test/headers/cli.doc