Plugin Commands: Green Power Test Device#

The Green Power Test Device plugin contributes CLI commands to the application framework to be used for generating commands from a GPD

Macros#

#define

plugin green-power-test-device send-ieee-test [gpdCommandId:1] [gpdCommandPayload:-1]

#define

plugin green-power-test-device send-test [gpdCommandId:1] [gpdCommandPayload:-1]

#define
#define

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_CHANNEL_REQUEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_CHANNEL_REQUEST

plugin green-power-test-device send-channel-request [channel:1]

  • Send a test GPD command

    • channel - INT8U - Channel to set


Definition at line 3422 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_COMM#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_COMM

plugin green-power-test-device send-comm [type:1]

  • Send a test GPD command

    • type - INT8U - 0 for tx only, 1 for bidir


Definition at line 3428 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_IEEE_TEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_IEEE_TEST

plugin green-power-test-device send-ieee-test [gpdCommandId:1] [gpdCommandPayload:-1]

  • Send a test GPD command

    • gpdCommandId - INT8U - gpd command ID

    • gpdCommandPayload - OCTET_STRING - gpd command payload


Definition at line 3435 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_TEST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_TEST

plugin green-power-test-device send-test [gpdCommandId:1] [gpdCommandPayload:-1]

  • Send a test GPD command

    • gpdCommandId - INT8U - gpd command ID

    • gpdCommandPayload - OCTET_STRING - gpd command payload


Definition at line 3442 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SET_PHY_CHANNEL#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SET_PHY_CHANNEL

plugin green-power-test-device set-phy-channel [channel:1]

  • set the phy channel

    • channel - INT8U - Channel to set


Definition at line 3448 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SETUP_GPD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SETUP_GPD

plugin green-power-test-device setup-gpd [srcId:4] [key:-1]

  • init a GPD

    • srcId - INT32U - gpd src ID

    • key - OCTET_STRING - the key


Definition at line 3455 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SETUP_IEEE_GPD#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SETUP_IEEE_GPD

plugin green-power-test-device setup-ieee-gpd [eui:-1] [key:-1]

  • init a Ieee GPD

    • eui - OCTET_STRING - gpd Ieee ID

    • key - OCTET_STRING - the key


Definition at line 3462 of file ./app/framework/test/headers/cli.doc