Plugin Commands: Interpan#
The Interpan commands provide commands to set global interpan state and test interpan fragmentation.
Macros#
plugin interpan disable
plugin interpan enable
plugin interpan fragment-test [panId:2] [eui64:8] [clusterId:2] [msgLen:2]
plugin interpan set-msg-timeout [timeout:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_DISABLE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_DISABLE
plugin interpan disable
Disables inter-PAN globally.
3737
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_ENABLE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_ENABLE
plugin interpan enable
Enables inter-PAN globally.
3742
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_FRAGMENT_TEST#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_FRAGMENT_TEST
plugin interpan fragment-test [panId:2] [eui64:8] [clusterId:2] [msgLen:2]
Sends a message of specified length of random values to target device over inter-PAN.
panId - INT16U - The PAN ID that the target is located on
eui64 - IEEE_ADDRESS - The target's EUI64 (big endian)
clusterId - INT16U - The cluster ID that the sample message should contain
msgLen - INT16U - The length of the randomly-filled message to be sent across inter-PAN
3751
of file ./app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_SET_MSG_TIMEOUT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_INTERPAN_PLUGIN_INTERPAN_SET_MSG_TIMEOUT
plugin interpan set-msg-timeout [timeout:1]
Sets the timeout for inter-PAN messages sent and received.
timeout - INT8U - Message timeout in seconds.
3757
of file ./app/framework/test/headers/cli.doc