Plugin Commands: Comms Hub Function (SubGhz)#

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_COMPLETE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_COMPLETE

plugin comms-hub-function-sub-ghz channel-change-complete [page:1] [channel:1]

  • Complete the channel change sequence.

    • page - INT8U - Requested new page [28-31]

    • channel - INT8U - Requested new channel


Definition at line 2173 of file ./app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_START#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_START

plugin comms-hub-function-sub-ghz channel-change-start

  • Initiate the channel change sequence.


Definition at line 2178 of file ./app/framework/test/headers/cli.doc