Api_network_mac_filter

Functions

gos_result_t gos_softap_mac_filter_add ( gos_mac_t *mac)
Add a MAC address to the MAC filter. More...
gos_result_t gos_softap_mac_filter_remove ( gos_mac_t *mac)
Remove a MAC address from the MAC filter. More...
gos_result_t gos_softap_mac_filter_clear (void)
Clear all addresses from MAC filter and disable filter. More...

Detailed Description

Function Documentation

gos_softap_mac_filter_add()

gos_result_t gos_softap_mac_filter_add ( gos_mac_t * mac )

Add a MAC address to the MAC filter.

Parameters
[in] mac MAC address to add to filter
Returns
result of api call, see gos_result_t

gos_softap_mac_filter_clear()

gos_result_t gos_softap_mac_filter_clear ( void )

Clear all addresses from MAC filter and disable filter.

Returns
result of api call, see gos_result_t

gos_softap_mac_filter_remove()

gos_result_t gos_softap_mac_filter_remove ( gos_mac_t * mac )

Remove a MAC address from the MAC filter.

Parameters
[in] mac MAC address to remove from filter
Returns
result of api call, see gos_result_t