Types
Event data types. More...
Enumerations | |
enum | gos_event_flag_t { GOS_EVENT_FLAG_NONE = 0, GOS_EVENT_FLAG_RUN_NOW = (1 << 0), GOS_EVENT_FLAG_ALLOW_DUPLICATE = (1 << 1), GOS_EVENT_FLAG_REQUIRE_WLAN = (1 << 3), GOS_EVENT_FLAG_REQUIRE_SOFTAP = (1 << 4), GOS_EVENT_FLAG_REQUIRE_ETHERNET = (1 << 5), GOS_EVENT_FLAG_IN_EVENT_THREAD = (1 << 6), GOS_EVENT_FLAG_IN_NETWORK_WORKER = (1 << 7), GOS_EVENT_FLAG_UPDATE_TIMEOUT = (1 << 8) } |
Event flags. More... | |
Detailed Description
Event data types.
Enumeration Type Documentation
◆ gos_event_flag_t
enum gos_event_flag_t |
Event flags.
Enumerator | |
---|---|
GOS_EVENT_FLAG_NONE | No event flags set. |
GOS_EVENT_FLAG_RUN_NOW | Run the event immediately (should be used with gos_event_register_periodic() ) |
GOS_EVENT_FLAG_ALLOW_DUPLICATE | Allow duplicate event handler. |
GOS_EVENT_FLAG_REQUIRE_WLAN | The event won't execute unless the GOS_INTERFACE_WLAN interface is up. |
GOS_EVENT_FLAG_REQUIRE_SOFTAP | The event won't execute unless the GOS_INTERFACE_SOFTAP interface is up. |
GOS_EVENT_FLAG_REQUIRE_ETHERNET | The event won't execute unless the GOS_INTERFACE_ETHERNET interface is up. |
GOS_EVENT_FLAG_IN_EVENT_THREAD | The event will execute in the system event thread (.
|
GOS_EVENT_FLAG_IN_NETWORK_WORKER | The event will execute in the networking work thread. |
GOS_EVENT_FLAG_UPDATE_TIMEOUT | Update a timed event's timeout if it's currently pending. |