String
Functions for processing strings. More...
Functions | |
char * | str_chop (char *haystack, const char *needle) |
Helper to find an occurrence of a delimiter string, insert '\0' in its place and return string after the delimiter. More... | |
int | str_isempty (const char *s) |
Check if string is non-null and non-empty. More... | |
int | str_isspace (const char *s) |
int | str_isnum (const char *s) |
int | str_isprint (const char *s) |
char * | str_reverse (char *s) |
char * | str_replace_all (char *s, const char *match_chars, char replace_char) |
char * | str_tolower (char *s) |
char * | str_toupper (char *s) |
char * | str_lstrip (char *s, const char *chars) |
Strip whitespace characters from the left Returns pointer into the input string. | |
char * | str_rstrip (char *s, const char *chars) |
Strip whitespace characters from the right Modified in place. | |
char * | str_strip (char *s, const char *chars) |
Combination of strip left + right. | |
gos_result_t | str_parse_base (const char *s, int base, intmax_t *result, intmax_t min, intmax_t max) |
gos_result_t | str_parse_int (const char *s, intmax_t *result, intmax_t min, intmax_t max) |
gos_result_t | str_parse_hex (const char *s, intmax_t *result, intmax_t min, intmax_t max) |
gos_result_t | str_parse_bool (const char *onoff, bool *var) |
void | str_binary_to_hex_buffer (char *hex_str, size_t hex_str_max_len, const void *binary_data, size_t binary_data_len) |
int | str_hex_to_binary (char *s) |
char * | str_binary_to_hex (void *binary_data, int binary_data_len) |
int | str_hex_to_byte (const char *hex_str) |
char * | str_byte_to_hex (uint8_t byte, char *hex_str) |
uint32_t | str_hex_to_uint32 (const char *hex_str) |
const char * | int32_to_str (int32_t i, char *str) |
const char * | uint32_to_str (uint32_t i, char *str) |
const char * | uint32_to_padded_str (uint32_t value, char *output, uint8_t max_padding) |
uint32_t | str_to_uint32 (const char *str) |
uint64_t | str_to_uint64 (const char *str) |
char * | uint64_to_str (const uint64_t uint64, char *str_buffer) |
const char * | bool_to_str (bool v) |
char * | strnstr (const char *haystack, const char *needle, size_t len) |
char * | strtok_r (char *, const char *, char **) |
gos_result_t | str_to_ipv4 (const char *ipstr, uint32_t *ipv4_ptr) |
const char * | ipv4_to_str (uint32_t ipv4, char *str_buffer) |
gos_result_t | str_to_ipv6 (const char *ipv6str, uint8_t *ipv6_ptr) |
const char * | ipv6_to_str (const uint8_t *ipv6, char *str_buffer) |
gos_result_t | str_to_ip (const char *ipstr, gos_ip_address_t *ip_address) |
const char * | ip_to_str (const gos_ip_address_t *ip_address, char *str_buffer) |
gos_result_t | str_to_mac (const char *mac_str, gos_mac_t *mac_buffer) |
char * | mac_to_str (const gos_mac_t *mac, char *str_buffer) |
const char * | ssid_to_str (gos_ssid_buffer_t buffer, const gos_ssid_t *ssid) |
float | str_to_float (const char *str) |
const char * | float_to_str (float f, char *str_buffer, uint8_t afterpoint) |
gos_result_t | str_buffer_pool_add (char *pool, uint16_t pool_len, const char *str, uint16_t *index) |
Add null-terminated string to string buffer pool. | |
gos_result_t | str_buffer_pool_add_with_len (char *pool, uint16_t pool_len, const char *str, int str_len, uint16_t *index) |
Add string of specified length to string buffer pool. | |
gos_result_t | str_buffer_pool_remove (char *pool, uint16_t pool_len, uint16_t index) |
Remove string a given index from string buffer pool. | |
Detailed Description
Functions for processing strings.
Function Documentation
◆ bool_to_str()
const char* bool_to_str | ( | bool | v | ) |
Convert boolean to string (true/false)
◆ float_to_str()
const char* float_to_str | ( | float | f, |
char * | str_buffer, |
||
uint8_t | afterpoint |
||
) |
Convert a float-point number to its string representation
- Parameters
-
f
Floating-point value str_buffer
Buffer to hold string representation afterpoint
Number of digits to print AFTER the decimal point
- Returns
- String value (same pointer as supplied
str_buffer
)
◆ int32_to_str()
const char* int32_to_str | ( | int32_t | i, |
char * | str |
||
) |
Convert int32 to string
◆ ip_to_str()
const char* ip_to_str | ( | const gos_ip_address_t * | ip_address, |
char * | str_buffer |
||
) |
Convert gos_ip_address_t to IPv4 or IPv6 string
◆ ipv4_to_str()
const char* ipv4_to_str | ( | uint32_t | ipv4, |
char * | str_buffer |
||
) |
Convert (host-byte-order) ipv4 to string (xxx.xxx.xxx.xxx)
- Examples:
- network/softap_tcp_server/main.c, and wifi/web_setup/main.c.
◆ ipv6_to_str()
const char* ipv6_to_str | ( | const uint8_t * | ipv6, |
char * | str_buffer |
||
) |
Convert ipv6 to string (xxxx:xxxx:xxxx:xxxx)
◆ mac_to_str()
char* mac_to_str | ( | const gos_mac_t * | mac, |
char * | str_buffer |
||
) |
Convert gos_mac_t to string (xx:xx:xx:xx:xx) str_buffer
must be at least 17 characters long
- Note
- If the
str_buffer
argument is NULL then an interal buffer is used. If thestr_buffer
argument is NULL then this API is NOT thread-safe.
◆ ssid_to_str()
const char* ssid_to_str | ( | gos_ssid_buffer_t | buffer, |
const gos_ssid_t * | ssid |
||
) |
Convert ssid to encoded string
- Examples:
- wifi/wifi_scan/main.c.
◆ str_binary_to_hex()
char* str_binary_to_hex | ( | void * | binary_data, |
int | binary_data_len |
||
) |
Destructively convert binary data into hex string The input binary_data buffer length MUST be at least binary_data_len*2 + 1 as the conversion is destructive and done in-place
◆ str_binary_to_hex_buffer()
void str_binary_to_hex_buffer | ( | char * | hex_str, |
size_t | hex_str_max_len, |
||
const void * | binary_data, |
||
size_t | binary_data_len |
||
) |
Convert binary data to hex string and put into destination buffer
◆ str_byte_to_hex()
char* str_byte_to_hex | ( | uint8_t | byte, |
char * | hex_str |
||
) |
Convert a byte to a padded hex char (XX)
◆ str_chop()
char* str_chop | ( | char * | haystack, |
const char * | needle |
||
) |
Helper to find an occurrence of a delimiter string, insert '\0' in its place and return string after the delimiter.
e.g.
- Parameters
-
haystack
The string to chop needle
String to find and split haystack on
- Returns
- Pointer to haystack after needle
◆ str_hex_to_binary()
int str_hex_to_binary | ( | char * | s | ) |
Destructively convert hex string to binary Returns number of bytes parsed or -1 on error. NOTE: The supplied input string is converted to binary in-place
◆ str_hex_to_byte()
int str_hex_to_byte | ( | const char * | hex_str | ) |
Convert hex string character to byte
◆ str_hex_to_uint32()
uint32_t str_hex_to_uint32 | ( | const char * | hex_str | ) |
Convert hex string to uint32
- Examples:
- demo/uart_blaster/uart_blaster.c.
◆ str_isempty()
int str_isempty | ( | const char * | s | ) |
Check if string is non-null and non-empty.
- Parameters
-
s
Pointer to string
- Returns
- 0 if the string is null or empty (i.e. only contains null-terminator), 1 else
◆ str_isnum()
int str_isnum | ( | const char * | s | ) |
Check is string contains all numeric characters
◆ str_isprint()
int str_isprint | ( | const char * | s | ) |
Check is string contains all printable characters
◆ str_isspace()
int str_isspace | ( | const char * | s | ) |
Check is string is all spaces
◆ str_parse_base()
gos_result_t str_parse_base | ( | const char * | s, |
int | base, |
||
intmax_t * | result, |
||
intmax_t | min, |
||
intmax_t | max |
||
) |
Parse based integer and check if it's in bounds [min, max].
◆ str_parse_bool()
gos_result_t str_parse_bool | ( | const char * | onoff, |
bool * | var |
||
) |
Parse string to boolean value
◆ str_parse_hex()
gos_result_t str_parse_hex | ( | const char * | s, |
intmax_t * | result, |
||
intmax_t | min, |
||
intmax_t | max |
||
) |
Parse hexadecimal integer and check if it's in bounds [min, max].
◆ str_parse_int()
gos_result_t str_parse_int | ( | const char * | s, |
intmax_t * | result, |
||
intmax_t | min, |
||
intmax_t | max |
||
) |
Parse integer and check if it's in bounds [min, max]. If string value starts with '0x' or '0X' then parse value as hex string (e.g.: base 16) If string value starts with '0b' or '0B' then parse value as binary string (e.g.: base 2)
◆ str_replace_all()
char* str_replace_all | ( | char * | s, |
const char * | match_chars, |
||
char | replace_char |
||
) |
Replace all matching characters in string with replacement character
◆ str_reverse()
char* str_reverse | ( | char * | s | ) |
Reverse characters in string in-place
◆ str_to_float()
float str_to_float | ( | const char * | str | ) |
Convert a string to a float
- Parameters
-
str
String representation of a floating point number
- Returns
- Converted float value
- Examples:
- test/throughput/throughput_cli_parser.c.
◆ str_to_ip()
gos_result_t str_to_ip | ( | const char * | ipstr, |
gos_ip_address_t * | ip_address |
||
) |
Convert IPv4 or IPv6 string to gos_ip_address_t
◆ str_to_ipv4()
gos_result_t str_to_ipv4 | ( | const char * | ipstr, |
uint32_t * | ipv4_ptr |
||
) |
Convert an ip string (xxx.xxx.xxx.xxx) to a uint32_t (host-byte-order).
◆ str_to_ipv6()
gos_result_t str_to_ipv6 | ( | const char * | ipv6str, |
uint8_t * | ipv6_ptr |
||
) |
Convert an ip string (xxxx:xxxx:xxxx:xxxx) to a ipv6 byte array.
◆ str_to_mac()
gos_result_t str_to_mac | ( | const char * | mac_str, |
gos_mac_t * | mac_buffer |
||
) |
Convert a MAC string (xx:xx:xx:xx:xx) or (xxxxxxxxxx) to a gos_mac_t
◆ str_to_uint32()
uint32_t str_to_uint32 | ( | const char * | str | ) |
Convert integer string to uint32 If string starts with '0x' parse as hex (e.g.: base 16) If string starts with '0b' parse as binary (e.g.: base 2)
◆ str_to_uint64()
uint64_t str_to_uint64 | ( | const char * | str | ) |
Convert integer string uint64 If string starts with '0x' parse has hex
◆ str_tolower()
char* str_tolower | ( | char * | s | ) |
Convert null-terminated string to lower case. ASCII charset only.
- Parameters
-
s
Pointer to string
- Returns
- Same pointer as argument with string converted to lowercase
◆ str_toupper()
char* str_toupper | ( | char * | s | ) |
Convert null-terminated string to upper case. ASCII charset only.
- Examples:
- hurricane/security_camera/main.c.
◆ strnstr()
char* strnstr | ( | const char * | haystack, |
const char * | needle, |
||
size_t | len |
||
) |
Returns a pointer to the first occurrence of needle in haystack, or a null pointer if needle is not part of haystack. Search no more than len characters of haystack.
- Examples:
- network/http_methods/main.c.
◆ strtok_r()
char* strtok_r | ( | char * | , |
const char * | , |
||
char ** | |
||
) |
◆ uint32_to_padded_str()
const char* uint32_to_padded_str | ( | uint32_t | value, |
char * | output, |
||
uint8_t | max_padding |
||
) |
Convert uint32 to string with '0' padding
◆ uint32_to_str()
const char* uint32_to_str | ( | uint32_t | i, |
char * | str |
||
) |
Convert uint32 to string
◆ uint64_to_str()
char* uint64_to_str | ( | const uint64_t | uint64, |
char * | str_buffer |
||
) |
Convert uint64 to string integer