Macros
Settings specific macros. More...
Macros | |
#define | GOS_VERIFY_SETTING_STR(setting, val) gos_settings_set_str(setting, val) |
Verify the result of setting a string setting, print message on failure. More... | |
#define | GOS_VERIFY_SETTING_UINT32(setting, val) gos_settings_set_uint32(setting, val) |
Verify the result of setting a uint32 setting, print message on failure. More... | |
#define | GOS_GET_SETTING_STR(setting, buffer) gos_settings_get_print_str(setting, buffer, sizeof(buffer)) |
Return a NVM setting as string. More... | |
Detailed Description
Settings specific macros.
Macro Definition Documentation
◆ GOS_GET_SETTING_STR
#define GOS_GET_SETTING_STR | ( | setting, |
|
buffer |
|||
) | gos_settings_get_print_str(setting, buffer, sizeof(buffer)) |
Return a NVM setting as string.
- Parameters
-
setting
The setting string to get buffer
Buffer to hold setting's string value
◆ GOS_VERIFY_SETTING_STR
#define GOS_VERIFY_SETTING_STR | ( | setting, |
|
val |
|||
) | gos_settings_set_str(setting, val) |
Verify the result of setting a string setting, print message on failure.
app must be built with debugging enabled for macro to take effect
◆ GOS_VERIFY_SETTING_UINT32
#define GOS_VERIFY_SETTING_UINT32 | ( | setting, |
|
val |
|||
) | gos_settings_set_uint32(setting, val) |
Verify the result of setting a uint32 setting, print message on failure.
app must be built with debugging enabled for macro to take effect